Power & Energy
  • Technologies
  • More
Power & Energy
Forum DC inverter doesn't power on Playstation4 when car is running. Why?
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 13 replies
  • Answers 8 answers
  • Subscribers 284 subscribers
  • Views 6994 views
  • Users 0 members are here
Related

DC inverter doesn't power on Playstation4 when car is running. Why?

iizeroxii
iizeroxii over 7 years ago

I have a dc inverter more than capable enough of powering the PlayStation 4. it works fine when the car is not running. When I start the car so the battery doesn't go flat the PS4 can't power on.

The vehicle is a Chrysler 300c 2013

the inverter is an Energizer 500W: https://www.energizerpower.com/product/en548/

Any idea as to why?

Would a capacitor/stiffening cap help?

  • Sign in to reply
  • Cancel

Top Replies

  • jw0752
    jw0752 over 7 years ago +5 suggested
    Hi Gavin, When the car is off the battery is a solid 12.6 volts and has a very low internal resistance so hooking up the inverter does not cause the voltage to drop much. When the car is running the alternator…
  • Gough Lui
    Gough Lui over 7 years ago +5 suggested
    As a rule of thumb, you should not have anything attached to the lighter socket during cranking. It's a bad idea since the transient from the starter motor can result in much lower and higher voltages…
  • iizeroxii
    iizeroxii over 7 years ago +4 suggested
    Ok so I found the problem. While the inverter was fine for the job. I agree that it should not be used while turning the engine. That was not the problem. The problem was that it doesn't work when the…
Parents
  • rusgray
    0 rusgray over 7 years ago

    Are you connecting the inverter through the cigarette lighter or are you using the clamps directly attached to the battery terminals?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • iizeroxii
    0 iizeroxii over 7 years ago in reply to rusgray

    Tried both the supplied cables, cigarette lighter and battery clamps, with the same results. Also tried some of my leftover amp power cables with proper terminals with the same results.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • rusgray
    0 rusgray over 7 years ago in reply to iizeroxii

    Does the PS4 shut down when you turn the engine over? Have you tried waiting ~30 seconds after starting the car to power the Playstation on again? Is there anything else attached to the inverter?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • iizeroxii
    0 iizeroxii over 7 years ago in reply to rusgray

    Yes, the PS4 shuts off when the engine is cracked. I have tried with just the PS4 plugged in, doesn't have any effect.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • iizeroxii
    0 iizeroxii over 7 years ago in reply to rusgray

    Also yes have waited for a little charge after starting the car.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • rusgray
    0 rusgray over 7 years ago in reply to iizeroxii

    Based on the information I was able to collect from a few quick online searches, the PS4 needs about 140W of power, and the cigarette adapter in most cars delivers around 180W. My guess is that when you start the engine, the voltage sags a bit, and likely takes some time to recover. During this low-voltage battery state, the inverter cannot deliver the power needed to supply the PS4. The inverter specs state a peak supply power of 1000W and a continuous power of 500W; based on what you've reported, either those specs are a lie (possible), or the PS4 consumes more than the stated 140W (also possible.) The inverter data sheet does not specify what the conversion efficiency is, so it's also possible that the voltage sag that happens during cranking pulls the amount of available power too low to run the PS4.

     

    If you have a high-current capable bench supply, you could try supplying the inverter with 12VDC from the bench supply and measure the current draw.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • iizeroxii
    0 iizeroxii over 7 years ago in reply to rusgray

    Thanks for the effort and information. But the thing is that I got this inverter because I have seen this same inverter being used to power a ps4. So I suspect it my vehicle that is the problem.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • iizeroxii
    0 iizeroxii over 7 years ago in reply to rusgray

    Thanks for the effort and information. But the thing is that I got this inverter because I have seen this same inverter being used to power a ps4. So I suspect it my vehicle that is the problem.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer