Power & Energy
  • Technologies
  • More
Power & Energy
Forum NiMH battery pack charger
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 5 replies
  • Answers 3 answers
  • Subscribers 284 subscribers
  • Views 1201 views
  • Users 0 members are here
  • battery controllers
  • nicd/nimh_battery_charger
Related

NiMH battery pack charger

koudelad
koudelad over 7 years ago

Hello,

 

About 10 years ago, all the major semiconductor manufacturers offered IC for battery management. Now looking at Texas Instruments, Maxim, Microchip and can't find a single device for charging a pack of 6 NiMH cells (industrial AAA cells) - 7.2 V, 600 - 750 mAh. The packs have an integrated NTC for temperature monitoring.

 

I have two use cases:

1) just a charger that will be able to charge them within ca. 2 hours (0.5 - 1 C with correct charge detection).

2) charger that will be able to charge the batteries and power a target device (ca. 50 - 100 mA power consumption) - that would be OK with a slow 0.1 C (a even a bit less). The slow charging alone could be easily done via LM317 etc. in constant current mode, but I have no idea how to handle the power consumption of the target device.

 

Any ideas? I would prefer either some relatively simple solution like LM317 or some specialized charger IC, but preferably with some ready-made evaluation board available.

 

Thank you,

David

  • Sign in to reply
  • Cancel

Top Replies

  • Gough Lui
    Gough Lui over 7 years ago +4 suggested
    You could try the MAX713 as well - https://www.maximintegrated.com/en/products/power/battery-management/MAX713.html - Gough
  • shabaz
    shabaz over 7 years ago +3 verified
    Hi David, I think it could be worth making one from scratch in that situation : ( As you say, the charger IC options are limited. Since it has integrated NTC, that's a nice way to (fairly) quickly detect…
  • luislabmo
    luislabmo over 7 years ago +3 suggested
    Have you explored the Maxim DS2715BZ+ Maxim DS2715BZ+ ?. It can handle up to 10 NiMH batteries and has FAST-CHARGE up to 2C, monitors voltage, temperature and time. In the datasheet there are couple of…
Parents
  • Gough Lui
    0 Gough Lui over 7 years ago

    You could try the MAX713 as well -

    https://www.maximintegrated.com/en/products/power/battery-management/MAX713.html

     

    - Gough

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • Gough Lui
    0 Gough Lui over 7 years ago

    You could try the MAX713 as well -

    https://www.maximintegrated.com/en/products/power/battery-management/MAX713.html

     

    - Gough

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer