Power & Energy
  • Technologies
  • More
Power & Energy
Forum Ring Connector - Consumer Application Help
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 7 replies
  • Answers 6 answers
  • Subscribers 284 subscribers
  • Views 1249 views
  • Users 0 members are here
Related

Ring Connector - Consumer Application Help

kzelectronics
kzelectronics over 7 years ago

I am trying to develop a conversion kit to connect competitors products to my controller.  Most of the products use wire connectors and I can easily develop a conversion wire with the appropriate connectors.  One of the products I am trying to convert has a ring terminal on the end of it.  I am trying to find a solution that the average consumer can clamp or insert the ring terminal into as part of my conversion kit.  I've attached a picture to show a mocked up converter and to show the ring terminal I'm trying to convert. 

 

Thank you for your ideas,

Kristine

Attachments:
image
  • Sign in to reply
  • Cancel

Top Replies

  • 14rhb
    14rhb over 7 years ago +4 suggested
    Hi Kristine, Any idea what voltage and current flow is expected on that lug? I think shabaz probably has the neatest and safest suggestion. I see your concern that not everyone will have the skills to…
  • three-phase
    three-phase over 7 years ago +4 suggested
    Another connector you may consider is a wire splice / insulation displacement connector. There are many available. Farnell wire splice range Something from the TE CoolSplice / 3M Scotchlok only requires…
  • dougw
    dougw over 7 years ago +3 suggested
    There are lots of ring terminal adapters on the market ranging from low-cost crimp connectors to something like this:
Parents
  • shabaz
    0 shabaz over 7 years ago

    Hi Kristine,

     

    One idea could be to suggest to customers to cut off the ring terminal, and supply this type of connector, Wago 222 seriesWago 222 series (as an example - there are other similar ones too).

    Otherwise you'd need some screw terminal block, and all that comes with it (the need to insulate it by placing it inside an enclosure). The Wago connector just needs the orange lever to be pushed up, the wire to be stripped, it is inserted into the connector and then the orange lever is pushed down.

     

    Also, if the customer keeps the cut ring terminal end, they can always go back to the previous state, by inserting that stripped ring terminal end into the Wago connector.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • shabaz
    0 shabaz over 7 years ago

    Hi Kristine,

     

    One idea could be to suggest to customers to cut off the ring terminal, and supply this type of connector, Wago 222 seriesWago 222 series (as an example - there are other similar ones too).

    Otherwise you'd need some screw terminal block, and all that comes with it (the need to insulate it by placing it inside an enclosure). The Wago connector just needs the orange lever to be pushed up, the wire to be stripped, it is inserted into the connector and then the orange lever is pushed down.

     

    Also, if the customer keeps the cut ring terminal end, they can always go back to the previous state, by inserting that stripped ring terminal end into the Wago connector.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • kzelectronics
    0 kzelectronics over 7 years ago in reply to shabaz

    Thank you - I'm still not sure I can expect the average consumer to be able to cut the wires and strip them, but I may need to try that.

     

    Kristine