Power & Energy
  • Technologies
  • More
Power & Energy
Forum Supercapacitor charging and discharging
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 10 replies
  • Answers 3 answers
  • Subscribers 282 subscribers
  • Views 1924 views
  • Users 0 members are here
  • supercapacitor
  • power
Related

Supercapacitor charging and discharging

oseania
oseania over 7 years ago

Hi,

 

Due to space constraints we have a very small battery (capacity around 20 mAh) which can provide max currents around 10 mA. However we would need short pulses (1 ms) of peak current (about 300mA) for about 1s. The only option that came to mind is to use supercapacitor as a secondary storage and drive the peak pulsed current from there. Would it be practical to use supercap for this kind of peaked discharging? Are there any dangers that we should consider?

  • Sign in to reply
  • Cancel

Top Replies

  • michaelkellett
    michaelkellett over 7 years ago in reply to oseania +4 suggested
    That's an average of 150mA for 1s. A 1F cap will drop 150mV, you need to decide how much drop you can stand and that will set the size of cap you need. Suppose you go for 0.5F and accept a 300mV drop in…
  • baldengineer
    baldengineer over 7 years ago +3
    we would need short pulses (1 ms) of peak current (about 300mA) for about 1s Do you need a 1ms pulse every 1s? Or you want to sustain 300mA for 1s? Or you want multiple of 1ms pulses for a 1s duration…
  • oseania
    oseania over 7 years ago in reply to michaelkellett +2
    Hi, The battery is a custom Li-Ion cell with 0.5C max discharge. It is very tiny, around 10x20mm. We use the battery to heat a resistive wire, so in that sense only the current counts, not the voltage…
Parents
  • baldengineer
    0 baldengineer over 7 years ago

    we would need short pulses (1 ms) of peak current (about 300mA) for about 1s

    Do you need a 1ms pulse every 1s? Or you want to sustain 300mA for 1s? Or you want multiple of 1ms pulses for a 1s duration? If the last one, then how many pulses in the 1s timeframe and how often does that 1s time frame occur.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • baldengineer
    0 baldengineer over 7 years ago

    we would need short pulses (1 ms) of peak current (about 300mA) for about 1s

    Do you need a 1ms pulse every 1s? Or you want to sustain 300mA for 1s? Or you want multiple of 1ms pulses for a 1s duration? If the last one, then how many pulses in the 1s timeframe and how often does that 1s time frame occur.

    • Cancel
    • Vote Up +3 Vote Down