Power & Energy
  • Technologies
  • More
Power & Energy
Forum TP5100 LiPo charging module failing
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 15 replies
  • Answers 8 answers
  • Subscribers 287 subscribers
  • Views 14000 views
  • Users 0 members are here
Related

TP5100 LiPo charging module failing

zagene
zagene over 7 years ago

Hi, I purchased 10 of the TP5100 modules trough Banggood and already six of them failed miserably. (With all of them the TP5100 IC failed)

The problem seems to be with some external components and I studied the circuit and the badly translated document so I redid the document as well as I could.

The main problem seems to be with the Schottky, the SS34’s reverse leakage current maybe just to high for the IC (or maybe sub-standard).

Im planning to replace it with MBRS540T3G with an reverse leakage of 300uA (any suggestions of a Schottky with a DO-214AB package size) as a replacement for the four that survived. I'm also going to replace the remaining three 10uF caps for just in case and also the 100nF cap. I’m going to use a low ESR 10uF cap from TDK with a 10% tolerance (C3216X7R1E106K160AB). All the components footprint is the same as the current. I’m also thinking about replacing the two 100 mOhm resistor with a 1% tolerance 50 mOhm 1W resistor (MCS1632R050FER) (Rs) that is specifically for current sense purposes just to be on the safe side (The modules takes way to long to reach me to risk the remaining four and with sensitive devices like the LiPo batteries make it high risk)

The NTC that is on the diagram is not avaiable on the module and seems to be tied to ground with RTRIC for a 10% trickle charge current. The on board LED also have some pads for an external two color LED (common anode) next to the input. The PWR_ON is left floating as in the diagram. To enable 8.4V (two cell charging) the SET pads may be linked to establish a link between CS and the reference voltage at VREG.

I have improved the translated document on the TP5100 and made some notes in PDF format If you are interested.

Could you please give comments about the suggested changes. I just hate to loose the last four modules as this seems to be and good charging module

image

image

  • Sign in to reply
  • Cancel

Top Replies

  • shabaz
    shabaz over 7 years ago +4 suggested
    Hi Eugene, This seems to be a LiPo battery charger module.. if six have already failed, I'd personally stay away from the remainder. If you can't have confidence in the design, it's not a good idea to…
  • genebren
    genebren over 7 years ago +4 suggested
    Hi Eugene, I am not sure that changing out the capacitors will be much help. They are there to help eliminate noise on the battery voltage sense and the charger output and would not likely cause the failures…
  • zagene
    zagene over 7 years ago +4 suggested
    Something else I failed to mention, The failure to the IC occurred even before I added the 18350 LiPo Cell It happened directly after I applied a 13.8V supply to the module. The supply is a Regulated step…
Parents
  • tankcircuit
    0 tankcircuit over 5 years ago

    It appears that you might be exceeding the maximum voltage as per the datasheet. There are two applications (single-cell 1S and dual-cell 2S), if pin 13 is not connected (one of the two "SET pads".), then the input charging voltage will range from 5-12VDC. I think I saw that you are applying over 13VDC.

    In the second application, pin 12 is shorted to pin 10 (the other pad of the "SET pads"). Now the input charge voltage can exceed this 12VDC threshold. With these pads shorted the IC will output 8.4VDC to charge two cells in series. I heard that the input voltage could be as low as 9.0VDC for the necessary headroom but that isn't specified in these diagrams.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • tankcircuit
    0 tankcircuit over 5 years ago

    It appears that you might be exceeding the maximum voltage as per the datasheet. There are two applications (single-cell 1S and dual-cell 2S), if pin 13 is not connected (one of the two "SET pads".), then the input charging voltage will range from 5-12VDC. I think I saw that you are applying over 13VDC.

    In the second application, pin 12 is shorted to pin 10 (the other pad of the "SET pads"). Now the input charge voltage can exceed this 12VDC threshold. With these pads shorted the IC will output 8.4VDC to charge two cells in series. I heard that the input voltage could be as low as 9.0VDC for the necessary headroom but that isn't specified in these diagrams.