Power & Energy
  • Technologies
  • More
Power & Energy
Forum Lead acid protection circuit
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 10 replies
  • Answers 6 answers
  • Subscribers 283 subscribers
  • Views 4210 views
  • Users 0 members are here
Related

Lead acid protection circuit

zagene
zagene over 7 years ago

Hi everyone,

I'm always looking for alternatives for a DC supply, as we have a constant problem with mains supply failure.

Add to this that I am a Ham operator who like to keep things up and running, even on DC power if required.

For DC supply I have the normal AC to DC switch mode supplies but the problem is with a suitable protection for my (very expensive according to me) AGM 12VDC batteries.

If you fail to constantly monitor the AGM battery output voltage or with swapping batteries accidentally (and it do happens if you are in a hurry at night) connect it reverse polarity you have a problem.

I have read many articles on battery protection especially with RPP and current flow back prevention as well as a battery low voltage cut-off so I'm starting a project that is compact and cost efficient enough to add to all my SLA's and AGM (and also all flooded cells for that matter) 12V batteries.

So my circuit is more a combination of several other circuits combining an efficient RPP without to many heat losses as well as combining it with a ATTiny ADC to read the voltage to cut off the battery at a preset low voltage, nothing very extravagant or to large or difficult to populate on a single sided PCB and fit it on the battery output.

My requirements would be to feed a radio or other load with DC at a maximum of 30A @ 13.8VDC (as required by my radio when transmitting.

The circuit area I'm not very sure of is the cut-off feed from the ATTiny45 via the 2N7000 that will cut the ground from the main P-ch MOSFET as a high side switch with a maximum current of 55A, Maximum gate voltage of 20V and a RDS(on) of 20mOhm at Vgs of -10VDC.

The second problem may be an Inrush current needed by the load which I do not totally want to limit as in certain instances my radio may require but I have to protect the MOSFET.

The other thing maybe to place a uni directional TVS at the battery poles of the circuit e.g. 1N6377 to clamp high voltage peaks etc.

Please advise me on the following circuit: (its available on PDF format here https://drive.google.com/drive/folders/1jG2ML2XMi52CiVaMMP-QXK-w0ViSZoYC?usp=sharing ) as well as the IRF4905 datasheet

image

  • Sign in to reply
  • Cancel

Top Replies

  • dougw
    dougw over 7 years ago +3 suggested
    Interesting application. You could also use something like an LTC4352 to create an ideal diode which also has under voltage protection. An alternative is LM74700.
  • jw0752
    jw0752 over 7 years ago +2 suggested
    Hi Eugene, You may want to check and verify the polarity of the IRF4905 as in its current config the internal Schottky will conduct current battery to load. As far as the rest of the design I will defer…
  • jw0752
    jw0752 over 7 years ago +2
    Hi Eugene, After reviewing the polarity protection application I believe I was wrong to question the polarity of the IRF 4905. It is correct as you have it. Sorry for the confusion but I have a little…
Parents
  • colporteur
    0 colporteur over 6 years ago

    Your post mentioned switching batteries. My commentary is not on the circuit but, on the batteries.

     

    My daughter has gutted and is retrofiring a 1983, 14ft travel trailer. I am currently building from the ground up, the electrical system, converter, fuse panel, wiring and battery.  I have discovered that using 2 X 6VDC batteries to achieve 12VDC is preferred over a single 12VDC battery.

     

    The information I have is anecdotal. Both the travel trailer vendor and a battery supply house recommends 6VDC batteries used in golf carts. They indicated the performance of recover time, number of charge cycles and the length they hold a charge is much better. The 6VDC battery has a demanding market, that the battery companies are focusing on.

     

    The other benefit they suggest is the reduce cost of replacing a battery. I would think you would replace both batteries if you were doing a replacement but that is just me.

     

    I have taken them up on their suggestion to use 6VDC batteries. I am still working on the trailer so I can't give you any field data that suggests the recommendation has some merit. When you think about it, golf carts seem to have a lot of getup and go and last a few beers at least going around the course.

     

    Sean

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • colporteur
    0 colporteur over 6 years ago

    Your post mentioned switching batteries. My commentary is not on the circuit but, on the batteries.

     

    My daughter has gutted and is retrofiring a 1983, 14ft travel trailer. I am currently building from the ground up, the electrical system, converter, fuse panel, wiring and battery.  I have discovered that using 2 X 6VDC batteries to achieve 12VDC is preferred over a single 12VDC battery.

     

    The information I have is anecdotal. Both the travel trailer vendor and a battery supply house recommends 6VDC batteries used in golf carts. They indicated the performance of recover time, number of charge cycles and the length they hold a charge is much better. The 6VDC battery has a demanding market, that the battery companies are focusing on.

     

    The other benefit they suggest is the reduce cost of replacing a battery. I would think you would replace both batteries if you were doing a replacement but that is just me.

     

    I have taken them up on their suggestion to use 6VDC batteries. I am still working on the trailer so I can't give you any field data that suggests the recommendation has some merit. When you think about it, golf carts seem to have a lot of getup and go and last a few beers at least going around the course.

     

    Sean

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer