Power & Energy
  • Technologies
  • More
Power & Energy
Forum Lead acid protection circuit
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 10 replies
  • Answers 6 answers
  • Subscribers 283 subscribers
  • Views 4210 views
  • Users 0 members are here
Related

Lead acid protection circuit

zagene
zagene over 7 years ago

Hi everyone,

I'm always looking for alternatives for a DC supply, as we have a constant problem with mains supply failure.

Add to this that I am a Ham operator who like to keep things up and running, even on DC power if required.

For DC supply I have the normal AC to DC switch mode supplies but the problem is with a suitable protection for my (very expensive according to me) AGM 12VDC batteries.

If you fail to constantly monitor the AGM battery output voltage or with swapping batteries accidentally (and it do happens if you are in a hurry at night) connect it reverse polarity you have a problem.

I have read many articles on battery protection especially with RPP and current flow back prevention as well as a battery low voltage cut-off so I'm starting a project that is compact and cost efficient enough to add to all my SLA's and AGM (and also all flooded cells for that matter) 12V batteries.

So my circuit is more a combination of several other circuits combining an efficient RPP without to many heat losses as well as combining it with a ATTiny ADC to read the voltage to cut off the battery at a preset low voltage, nothing very extravagant or to large or difficult to populate on a single sided PCB and fit it on the battery output.

My requirements would be to feed a radio or other load with DC at a maximum of 30A @ 13.8VDC (as required by my radio when transmitting.

The circuit area I'm not very sure of is the cut-off feed from the ATTiny45 via the 2N7000 that will cut the ground from the main P-ch MOSFET as a high side switch with a maximum current of 55A, Maximum gate voltage of 20V and a RDS(on) of 20mOhm at Vgs of -10VDC.

The second problem may be an Inrush current needed by the load which I do not totally want to limit as in certain instances my radio may require but I have to protect the MOSFET.

The other thing maybe to place a uni directional TVS at the battery poles of the circuit e.g. 1N6377 to clamp high voltage peaks etc.

Please advise me on the following circuit: (its available on PDF format here https://drive.google.com/drive/folders/1jG2ML2XMi52CiVaMMP-QXK-w0ViSZoYC?usp=sharing ) as well as the IRF4905 datasheet

image

  • Sign in to reply
  • Cancel

Top Replies

  • dougw
    dougw over 7 years ago +3 suggested
    Interesting application. You could also use something like an LTC4352 to create an ideal diode which also has under voltage protection. An alternative is LM74700.
  • jw0752
    jw0752 over 7 years ago +2 suggested
    Hi Eugene, You may want to check and verify the polarity of the IRF4905 as in its current config the internal Schottky will conduct current battery to load. As far as the rest of the design I will defer…
  • jw0752
    jw0752 over 7 years ago +2
    Hi Eugene, After reviewing the polarity protection application I believe I was wrong to question the polarity of the IRF 4905. It is correct as you have it. Sorry for the confusion but I have a little…
Parents
  • dougw
    0 dougw over 7 years ago

    Interesting application.

    You could also use something like an LTC4352 to create an ideal diode which also has under voltage protection.

    An alternative is LM74700.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • zagene
    0 zagene over 6 years ago in reply to dougw

    Hi Douglas

    I researched quite a lot on the ideal diode controller bu because of reasons mentioned below I could not continue, but I stumbled on another similar controller that is locally available at a much more competitive price range but some things is not very clear. Can you please help me here.

    Here is part of my circuit of the ZXGD3112N7TC ideal diode controller (SOIC package 127mil in stead of 65mil or 50mil that would be much better to prototype by hand) see https://www.diodes.com/assets/Datasheets/ZXGD3112N7.pdf

     

    image

    From the datasheet I gather that the PWR GND and GND is referenced to the same source ground to probably accommodate the driving of the N-channel MOSFET. It differs quite a lot from the Ideal Diode controllers of Linear Technology (the documents of LT also better explanatory than the one of Diodes Inc) see Figure 4 on page 6 of the above document.

    As from this figure the VCC should be from another resource probably a linear regulator if the source voltage is higher than the maximum VCC of the device which is 25V, but still referenced to the device ground which is the source voltage and seemingly not the system ground or input ground.

    Since the probability of a DC 12V supply (14.4VDC max) is not above the maximum rating of VCC, then the zener is most probably not necessary, but again, referenced to what ground? I'm a bit confused here.

    Ive looked at other similar devices and all of them only have a 100n cap between the VCC and device ground (the devices with a ground referenced to the source level). What about a charge pump for the gate drive. Is it not needed.

    LTC4357's IN pin is maybe similar to this devices GND pin but with the LTC4357 the device GND is protected by a bidirectional transzorb between the source and system Ground with a Dclamp zener (Uni Directional transzorb) between drain and the device ground to limit the overall device voltage to a VDD level lower than the operating supply range. Would the ZXGD3112N7TC circuit then be similar than the circuit of the LTC4357 on page 10 marked Reverse Input Protection. I'm not entirely sure about the ZXGD3112N7TC's VCC supply level, or maybe I should just use the 100n cap in this instance but what about unexpected transient spikes. This could aid me quite a lot with multiple outputs ORing.

    (See https://www.analog.com/media/en/technical-documentation/data-sheets/4357fd.pdf on page 10)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • zagene
    0 zagene over 6 years ago in reply to dougw

    Hi Douglas

    I researched quite a lot on the ideal diode controller bu because of reasons mentioned below I could not continue, but I stumbled on another similar controller that is locally available at a much more competitive price range but some things is not very clear. Can you please help me here.

    Here is part of my circuit of the ZXGD3112N7TC ideal diode controller (SOIC package 127mil in stead of 65mil or 50mil that would be much better to prototype by hand) see https://www.diodes.com/assets/Datasheets/ZXGD3112N7.pdf

     

    image

    From the datasheet I gather that the PWR GND and GND is referenced to the same source ground to probably accommodate the driving of the N-channel MOSFET. It differs quite a lot from the Ideal Diode controllers of Linear Technology (the documents of LT also better explanatory than the one of Diodes Inc) see Figure 4 on page 6 of the above document.

    As from this figure the VCC should be from another resource probably a linear regulator if the source voltage is higher than the maximum VCC of the device which is 25V, but still referenced to the device ground which is the source voltage and seemingly not the system ground or input ground.

    Since the probability of a DC 12V supply (14.4VDC max) is not above the maximum rating of VCC, then the zener is most probably not necessary, but again, referenced to what ground? I'm a bit confused here.

    Ive looked at other similar devices and all of them only have a 100n cap between the VCC and device ground (the devices with a ground referenced to the source level). What about a charge pump for the gate drive. Is it not needed.

    LTC4357's IN pin is maybe similar to this devices GND pin but with the LTC4357 the device GND is protected by a bidirectional transzorb between the source and system Ground with a Dclamp zener (Uni Directional transzorb) between drain and the device ground to limit the overall device voltage to a VDD level lower than the operating supply range. Would the ZXGD3112N7TC circuit then be similar than the circuit of the LTC4357 on page 10 marked Reverse Input Protection. I'm not entirely sure about the ZXGD3112N7TC's VCC supply level, or maybe I should just use the 100n cap in this instance but what about unexpected transient spikes. This could aid me quite a lot with multiple outputs ORing.

    (See https://www.analog.com/media/en/technical-documentation/data-sheets/4357fd.pdf on page 10)