Power & Energy
  • Technologies
  • More
Power & Energy
Forum How to Reduce low AC voltage
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 8 replies
  • Answers 4 answers
  • Subscribers 284 subscribers
  • Views 16531 views
  • Users 0 members are here
  • low voltage
  • step down
  • transformer
  • ac voltage
Related

How to Reduce low AC voltage

cricket-15
cricket-15 over 6 years ago

not sure this is the correct place to ask this or not but here goes, i have a 3 amp 120 volt AC step-down transformer to 20 volt AC, i want to reduce the 20 volts to 10 volts AC, i tried splitting it with two 50 watt resistors but they get very hot without a load, how can i reduce the 20 volt AC to 10 volt AC?

 

i've attached a picture of the transformer. any help i can get will be greatly appreciated.

Attachments:
image
  • Sign in to reply
  • Cancel

Top Replies

  • dougw
    dougw over 6 years ago +4 suggested
    There are several options - the first one is probably the least work: Obtain a transformer that converts 120 vac to 10 vac Use a second transformer to convert 20 vac to 10 vac Convert to DC and use an…
  • cricket-15
    cricket-15 over 6 years ago in reply to dougw +1 suggested
    here's what i'm trying to do, i want to use it for Etching and Marking of metals, I've converted the 20VAC to DC, the output DC volts are higher than the AC volts, it works as i have it set up today but…
  • beacon_dave
    beacon_dave over 6 years ago +1 suggested
    I think you bought the wrong train set... Lionel appear to do a hobby transformer with split variable outputs: CW-80 80-Watt Transformer
Parents
  • dougw
    0 dougw over 6 years ago

    There are several options - the first one is probably the least work:

    1. Obtain a transformer that converts 120 vac to 10 vac
    2. Use a second transformer to convert 20 vac to 10 vac
    3. Convert to DC and use an oscillator to generate 10 vac
    4. Install a series resistor equal to the load impedance, so half the voltage is across the resistor and half across the load
    5. Install a series resistor equal to the load impedance followed by back-to-back Zener diodes to clamp the output to 10 vac
    6. Run a 120 vac motor connected to a 10 vac generator
    7. Install back-to-back Zener diodes in series to reduce to voltage across the load (they will have to dissipate significant power and they distort the waveform)
    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • colporteur
    0 colporteur over 6 years ago in reply to dougw

    What about half rectifying instead of full rectifying. Doesn't that impact output voltage? Old man using his old electronics knowedge.

     

    Sean

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • colporteur
    0 colporteur over 6 years ago in reply to dougw

    What about half rectifying instead of full rectifying. Doesn't that impact output voltage? Old man using his old electronics knowedge.

     

    Sean

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer