Power & Energy
  • Technologies
  • More
Power & Energy
Forum Bridge rectifier magic?
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 10 replies
  • Answers 2 answers
  • Subscribers 283 subscribers
  • Views 2103 views
  • Users 0 members are here
Related

Bridge rectifier magic?

johnnybraveau
johnnybraveau over 6 years ago

Good morning. First-time newbie here. 2 years ago I yanked all the fluorescent fixtures from my shop and replaced them with LED strips, powered by cheap Chinese power supplies, see below (120VAC>12VDC, 30A).

Some have begun to fail, and so I bought some new  ones - exact replacements - and am using one as a standard against which to compare values, and help deduce faulty components. (not that I don’t have some clear “winners” already, i. e. swollen caps, blown thermistors).

But here’s where it gets goofy: in the process of sampling voltages on the “good” unit, I discovered that DC voltages aft of the bridge rectifier (GBU6J, GBU808, GBU810GBU810, or GBU406GBU406, depending on which board) are 2.75 times that of the AC input. Specifically, I’m getting 330VDC on the back side, with 120VAC going in. I’m including a picture of a “deduced” schematic - up to a point - along with the board itself. Power flows - on the board - from bottom left, anticlockwise around to top left. On the hand-written schematic, C1 and C6 are too small to read, so they got the “teeninie” designation, and probably don’t figure into the puzzle anyway. The pin-out of the semiconductors (2SC2625) after the 680uF electrolytic caps I am not certain of, and so I did not assign a collector/emitter, but based on their description on the spec sheet (“high power, high speed”) I am assuming this is where the 330VDC is chopped up (or modulated) and processed back into AC. The transformer represented by the “?” is the one all the way to the right on the board, nestled behind the big 680uF caps. I can’t begin to guess at the pinouts on that, but there are 3 terminals on one side, and 5 on the other.

 

so, to reiterate: 120VAC to 330VDC...?

 

As Professor Quirrell once said “What magic is this?”image

  • Sign in to reply
  • Cancel

Top Replies

  • dougw
    dougw over 6 years ago +2 verified
    For a sine wave 120 Vac RMS = 339.4 V peak-to-peak It sounds like you are measuring the peak-to-peak voltage.
  • johnnybraveau
    johnnybraveau over 6 years ago in reply to dougw +2
    I would hope the answer to be as simple (as my ignorance). I was raised to believe that what was coming out of the outlet (here in the US Colonies) is 60hz, 120VAC, peak to peak. So you’re telling me that…
  • colporteur
    colporteur over 6 years ago +1
    G'Day, I am going to speculate from the picture the unit is a switching power supply. The Difference Between a Linear Supply and a Switched Mode Power Supply Switching mode P.S. operate differently than…
Parents
  • dougw
    0 dougw over 6 years ago

    For a sine wave

    120 Vac RMS = 339.4 V peak-to-peak

    It sounds like you are measuring the peak-to-peak voltage.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • johnnybraveau
    0 johnnybraveau over 6 years ago in reply to dougw

    I would hope the answer to be as simple (as my ignorance). I was raised to believe that what was coming out of the outlet (here in the US Colonies) is 60hz, 120VAC, peak to peak.
    So you’re telling me that is not the case? (That it’s really 120V rms?)

    Or am I still missing the point?

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • johnnybraveau
    0 johnnybraveau over 6 years ago in reply to dougw

    I would hope the answer to be as simple (as my ignorance). I was raised to believe that what was coming out of the outlet (here in the US Colonies) is 60hz, 120VAC, peak to peak.
    So you’re telling me that is not the case? (That it’s really 120V rms?)

    Or am I still missing the point?

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • dougw
    0 dougw over 6 years ago in reply to johnnybraveau

    Yes, the mains ac voltage is always specified as an RMS value - even in the colonies. image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer