Power & Energy
  • Technologies
  • More
Power & Energy
Forum Possible to charge one battery to another battery?
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 9 replies
  • Answers 5 answers
  • Subscribers 282 subscribers
  • Views 20187 views
  • Users 0 members are here
  • Alternative Energy Tags
  • battery
  • energy
  • energy_power
  • energy_storage
Related

Possible to charge one battery to another battery?

hardik.jani
hardik.jani over 6 years ago

Hello connection 

 

 

I need your help regarding possible to charge one battery to another battery?

 

 

The requirement is if in our one battery dead then we might be not able to connect charger because we don't have AC plug at all places.

 

 

So the idea is there is another 2nd battery which can charge the battery in an emergency situation

 

 

Battery Specification:-

 

 

25.9 V 60 Ah

Lithium iron cell (18650) 7 cell in serise 24 cell in perellel

Charge mode:CC/CV

Charge Voltage:-29.4±0.02V

Nominal Voltage :- 25.9V

Capacity :- 60Ah

Discharge Cut-off Voltage :-19.25V

 

 

My question is can we able to charge one battery to another same battery?

 

 

Kindly share your valuable input regarding this question

  • Sign in to reply
  • Cancel

Top Replies

  • michaelkellett
    michaelkellett over 6 years ago +4 suggested
    A good system would not attempt to charge the empty or failed battery from the back up battery(which will always waste energy and in the case of a failed main battery will not work at all). You should…
  • Pavel.Simon
    Pavel.Simon over 6 years ago +2 suggested
    Generaly you can charge "empty" battery with the same "full" one. But question is not about empty (or discharged) battery against full (or fully carged) battery. You write: " if in our one battery dead…
  • hardik.jani
    hardik.jani over 6 years ago +1
    Hello All, Thanks for your reply. Let me clear more details. Basically we have made AGV for industrial application and it has 60Ah li-ion battery. So Thought point behind this requirement is some how battery…
Parents
  • Pavel.Simon
    0 Pavel.Simon over 6 years ago

    Generaly you can charge "empty" battery with the same "full" one.

     

    But question is not about empty (or discharged) battery against full (or fully carged) battery.
    You write: "if in our one battery dead" - if you mean empty (or discharged) then you can. Even you do not need charger or any electronics in betwen two batteries. You connect those batteries and energy will flow itself. Only you need to control  when current isstill flowing fron new to old... If it stops, you need to disconnect - chcrging would not be possible anymore. At that time you need to charge your new one to be able give energy to old one.

    Efficiency will not be good, but you can. More effective way is to replace one battery (empty one) with another (full one). Is it possible to physically change them?
    Hovewer different situation is if the battery is really dead. Then it will not work. Old dead battery would not be able to recieve any energy, and then you cannot charge it in any way. Then replacement is only way.

    Easy way is imagine it as two bottles: full one is able filling empty one. But any full one is not able fill broken (dead) one.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • hardik.jani
    0 hardik.jani over 6 years ago in reply to Pavel.Simon

    Hello Pavel Simon,

     

    Thank you for your reply!!!!!

     

    "The requirement is if in our one battery dead then we might be not able to connect charger because we don't have AC plug at all places."

     

    Ans:- the fully dead means  battery voltage is  23 V or 20 V and already integrated BMS circuit inside

     

    Que:- my question is would need any isolate or protection circuit need between two batteries?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • Pavel.Simon
    0 Pavel.Simon over 6 years ago in reply to hardik.jani

    for an emergency - no, but you need to control energy flow...

    for regular use - of course, yes

     

    so many other details are there:

    1. are there load in the process?

    2. any "strange" condition - humidity, temperature (high,low), ... - involved?

    3. value of devices in load?

     

    All of them is important in an estimate of protection. But really general are two rows of the beginning of this answer.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • Pavel.Simon
    0 Pavel.Simon over 6 years ago in reply to hardik.jani

    for an emergency - no, but you need to control energy flow...

    for regular use - of course, yes

     

    so many other details are there:

    1. are there load in the process?

    2. any "strange" condition - humidity, temperature (high,low), ... - involved?

    3. value of devices in load?

     

    All of them is important in an estimate of protection. But really general are two rows of the beginning of this answer.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer