Power & Energy
  • Technologies
  • More
Power & Energy
Forum Possible to charge one battery to another battery?
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 9 replies
  • Answers 5 answers
  • Subscribers 282 subscribers
  • Views 20190 views
  • Users 0 members are here
  • Alternative Energy Tags
  • battery
  • energy
  • energy_power
  • energy_storage
Related

Possible to charge one battery to another battery?

hardik.jani
hardik.jani over 6 years ago

Hello connection 

 

 

I need your help regarding possible to charge one battery to another battery?

 

 

The requirement is if in our one battery dead then we might be not able to connect charger because we don't have AC plug at all places.

 

 

So the idea is there is another 2nd battery which can charge the battery in an emergency situation

 

 

Battery Specification:-

 

 

25.9 V 60 Ah

Lithium iron cell (18650) 7 cell in serise 24 cell in perellel

Charge mode:CC/CV

Charge Voltage:-29.4±0.02V

Nominal Voltage :- 25.9V

Capacity :- 60Ah

Discharge Cut-off Voltage :-19.25V

 

 

My question is can we able to charge one battery to another same battery?

 

 

Kindly share your valuable input regarding this question

  • Sign in to reply
  • Cancel

Top Replies

  • michaelkellett
    michaelkellett over 6 years ago +4 suggested
    A good system would not attempt to charge the empty or failed battery from the back up battery(which will always waste energy and in the case of a failed main battery will not work at all). You should…
  • Pavel.Simon
    Pavel.Simon over 6 years ago +2 suggested
    Generaly you can charge "empty" battery with the same "full" one. But question is not about empty (or discharged) battery against full (or fully carged) battery. You write: " if in our one battery dead…
  • hardik.jani
    hardik.jani over 6 years ago +1
    Hello All, Thanks for your reply. Let me clear more details. Basically we have made AGV for industrial application and it has 60Ah li-ion battery. So Thought point behind this requirement is some how battery…
Parents
  • e14 Contributor
    e14 Contributor over 4 years ago
    This reply was deleted.
    • Cancel
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 4 years ago
    This reply was deleted.
    • Cancel
    • Cancel
Children
  • Jan Cumps
    0 Jan Cumps over 4 years ago in reply to e14 Contributor

    Spam in white font. Go figure