Power & Energy
  • Technologies
  • More
Power & Energy
Forum Power sensing circuit
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 9 replies
  • Answers 3 answers
  • Subscribers 283 subscribers
  • Views 2327 views
  • Users 0 members are here
Related

Power sensing circuit

pjshah72
pjshah72 over 6 years ago

Hi All,

 

I am with EE back-ground and recently I had question in interview regarding “How to sense/know when device needs power?”.


So, basically I had a good interview on different topics and one of them was MOSFET.
I answered mostly all questions properly until this question comes up.
Interviewer asked me: “If you are making power supply for a laptop and when laptop goes in to sleep that time your supply should not provide full power (may be negligible). And when you on the laptop or started working on it at that time your supply should provide required power.”
How can you design circuit which sense/detects when device needs power?

 

Can any one of you help me on this? I would really appreciated any input.


Thank you,

pj

  • Sign in to reply
  • Cancel

Top Replies

  • dougw
    dougw over 6 years ago +2 suggested
    It sounds like you need to start with a sensor that detects when the computer needs power and when it doesn't. Many laptops have a switch that senses when the display/lid closes and generates a signal…
  • jw0752
    jw0752 over 6 years ago +2 suggested
    Hi Pujan, I am not an expert but it seems to me that this may have been a trick question. If the electronics of the computer are making the decision to go into sleep or low power mode does the power supply…
  • pjshah72
    pjshah72 over 6 years ago in reply to dougw +2
    Thank you Douglas Wong for your detailed reply. I completely understood what you have mentioned related to signal which controlled through CPU and that drives power supply. Now next question to follow…
Parents
  • stefan.rosu
    0 stefan.rosu over 6 years ago

    Hi Pujan,

     

    If the question is related to a MOSFET in a laptop power supply then it is about switching and efficiency.

    A MOSFET in the power supply is switching ON or OFF at the switching frequency, lets say 100kHz. This will generate losses that are present even at low output current.

    The MOSFET is not jut by itself, it is controlled by a controller, analog or digital. The controller will keep the voltage constant at the output when the current is changing. The controller can have (or not) an enable input. Also, the output of the power supply has a capacitor so that even if the MOSFET will stop switching, the output voltage will decrease slowly, depending on the current drawn from the laptop.

    In order to increase the efficiency, when the laptop enters sleep and the supply current will drop below a small value, let say 10%, you can stop the MOSFET from switching to save power. Once this happens, the output voltage will start to decrease, but slow because the current is below 10%, so you can wait some time. When the voltage drops below a set value, let say 95% of nominal, then you start the MOSFET again, the voltage rises to the nominal value.

    There are several ways to implement this circuit in a generic way, that is, if it was not included in the controller already.

    The easy way is with a comparator with hysteresis that will generate a enable signal when the voltage is at 95% and disable when the voltage is at 100% (enable "0" or "1" logic).

    This may not be desirable at high power because you will always have a 5% voltage ripple at the output.

    To resolve this you need another comparator and a current sense resistor in the GND wire. The 2nd comparator will generate a signal when the output current is smaller than 10%. This signal can be an enable for the first comparator so that only when the current is smaller than 10% the voltage will be allowed to drop to 95% while the MOSFET is not switching.

    If the controller does not have an Enable pin, then you can use the same principle but you can act directly on the feedback pin of the controller, basically you will change the nominal voltage from 95% to 100% with a comparator by adding resistance in the feedback divider of the controller.

    This control can disable the MOSFET for long periods of time if the current in the laptop is very small. You can have also other means of communication between the laptop and power supply but this is about how to sense the power.

     

    Regards,

    Stefan

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • stefan.rosu
    0 stefan.rosu over 6 years ago

    Hi Pujan,

     

    If the question is related to a MOSFET in a laptop power supply then it is about switching and efficiency.

    A MOSFET in the power supply is switching ON or OFF at the switching frequency, lets say 100kHz. This will generate losses that are present even at low output current.

    The MOSFET is not jut by itself, it is controlled by a controller, analog or digital. The controller will keep the voltage constant at the output when the current is changing. The controller can have (or not) an enable input. Also, the output of the power supply has a capacitor so that even if the MOSFET will stop switching, the output voltage will decrease slowly, depending on the current drawn from the laptop.

    In order to increase the efficiency, when the laptop enters sleep and the supply current will drop below a small value, let say 10%, you can stop the MOSFET from switching to save power. Once this happens, the output voltage will start to decrease, but slow because the current is below 10%, so you can wait some time. When the voltage drops below a set value, let say 95% of nominal, then you start the MOSFET again, the voltage rises to the nominal value.

    There are several ways to implement this circuit in a generic way, that is, if it was not included in the controller already.

    The easy way is with a comparator with hysteresis that will generate a enable signal when the voltage is at 95% and disable when the voltage is at 100% (enable "0" or "1" logic).

    This may not be desirable at high power because you will always have a 5% voltage ripple at the output.

    To resolve this you need another comparator and a current sense resistor in the GND wire. The 2nd comparator will generate a signal when the output current is smaller than 10%. This signal can be an enable for the first comparator so that only when the current is smaller than 10% the voltage will be allowed to drop to 95% while the MOSFET is not switching.

    If the controller does not have an Enable pin, then you can use the same principle but you can act directly on the feedback pin of the controller, basically you will change the nominal voltage from 95% to 100% with a comparator by adding resistance in the feedback divider of the controller.

    This control can disable the MOSFET for long periods of time if the current in the laptop is very small. You can have also other means of communication between the laptop and power supply but this is about how to sense the power.

     

    Regards,

    Stefan

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • pjshah72
    0 pjshah72 over 6 years ago in reply to stefan.rosu

    Thank you so much Stefan for an excellent information and your way of explaining. I would definitely like to try this out (at-least simulation).

    I really appreciate your time. Do you have any good informative material on PMIC? If so, could you refer me?

     

    Thank you and stay safe,

    Pujan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • stefan.rosu
    0 stefan.rosu over 6 years ago in reply to pjshah72

    Hi Pujan,

     

    I think the best way to find up to date information about PMIC is to follow the integrated circuit image

    That is, you can explore the offering of Farnell for example, and see what type of PMIC they have available. You can see some classification, for example DC-DC, off-line, controller with or without integrated power transistors, etc. You find the datasheet and the manufacturer this way.

    One other way is to go directly to the IC manufacturer sites (like Vishay, STMicroelectronics, Texas Instruments,  ONSemi) and browse the converter categories. You will find there also additional materials like application notes.

     

    Regards,

    Stefan