Power & Energy
  • Technologies
  • More
Power & Energy
Forum Design of a low voltage and high current DC-DC converter
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 13 replies
  • Answers 3 answers
  • Subscribers 284 subscribers
  • Views 5757 views
  • Users 0 members are here
  • dc-dc converters
Related

Design of a low voltage and high current DC-DC converter

s1m0n3t
s1m0n3t over 6 years ago

Hi all,

I'm dealing with a quite strange design. I have a single 5V power source with few amps of current (about 3A) and I need to drive a load (about 0.8mOhm of resistance, but variable in function of voltage/current) with a current from -10A to 10A, at 100mV of maximum voltage.

I'm searching for an IC which can help me, but I don't found any suitable device, at this moment.

I would try a discrete configuration like the following schematic:

image

I can send an alternate (square wave) current with one or another direction in the transformer, using a PWM signal on CTRL1 or CTRL2, with 50% duty cycle.

If i use a 10:1 ratio transformer (for example), I will have a reduced maximum voltage, but with more current (about 10 times). Correct?

And then, with another PWM on CTRL3 or CTRL4, I can modulate the output from zero to positive maximum and to negative minimum voltage, measuring the voltage to the feedback point, or the current in series of the load (R1) with an hall effect sensor.

I probably don't even need two input windings, but I can send a single square wave in input and activate Q3 or Q4 to obtain a positive or negative output. And perhaps one of the two outgoing mosfets should be type P?

What do you think about this solution? Anyone have alternative ideas or suggestions?

  • Sign in to reply
  • Cancel

Top Replies

  • Jan Cumps
    Jan Cumps over 6 years ago +1
    Is the 100 mV a maximum, or a constant desired voltage? edit: reading the post again and the schematic, it looks like you want a swinging or switcheable output voltage between -100 and +100 mV? There's…
  • s1m0n3t
    s1m0n3t over 6 years ago in reply to Jan Cumps +1
    100mV is only a maximum, I need to regulate the current, so the voltage will depend on the load.
  • Jan Cumps
    Jan Cumps over 6 years ago in reply to s1m0n3t +1 suggested
    Can I summarise it like this? - you need a device that can control a DC current between -10 A and + 10 A. That current has to be configurable and maintained by the circuit. - it's derived from the load…
Parents
  • Jan Cumps
    0 Jan Cumps over 6 years ago

    Is the 100 mV a maximum, or a constant desired voltage?

     

    edit: reading the post again and the schematic, it looks like you want a swinging or switcheable output voltage between -100 and +100 mV?

    There's a few things to take into account:

    - even with low Ron for the secondary fets, the voltage drop is going to be significant at 10 A. In particular in relation to the 100 mV output.

    - the output capacitor needs to filter ripple on a 10 A signal, and it has to be bipolar - that may be hard to find. It may be better to outsource the majority of the ripple filtering to an inductor. But then that makes polarity shifting tricky ....

     

     

    I have a 48 V to 0.5 V design here (but without polarity selection on the secondary side). And it uses a number of measures to get to  a reasonable efficiency.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • s1m0n3t
    0 s1m0n3t over 6 years ago in reply to Jan Cumps

    100mV is only a maximum, I need to regulate the current, so the voltage will depend on the load.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • s1m0n3t
    0 s1m0n3t over 6 years ago in reply to Jan Cumps

    100mV is only a maximum, I need to regulate the current, so the voltage will depend on the load.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • Jan Cumps
    0 Jan Cumps over 6 years ago in reply to s1m0n3t

    Can I summarise it like this?

     

    - you need a device that can control a DC current between -10 A and + 10 A. That current has to be configurable and maintained by the circuit.

    - it's derived from the load that within these ranges, the output voltage will stay between -100 mV and 100 mV

    - The input voltage has to be 5 V DC.

    - a switch mode design.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • s1m0n3t
    0 s1m0n3t over 6 years ago in reply to Jan Cumps

    Correct