Power & Energy
  • Technologies
  • More
Power & Energy
Forum How to sense mains AC?
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 8 replies
  • Answers 2 answers
  • Subscribers 283 subscribers
  • Views 1871 views
  • Users 0 members are here
Related

How to sense mains AC?

johninjax
johninjax over 6 years ago

Hey,

I need to know if a latching SPDT relay is on the A or B side. The relay has a 5V control, but it will have 120VAC on it. I was planning to use a half wave rectifier and RC filter with large R to tap off ~5V into a gate. Am I crazy? Is there a better/simpler way?

 

Thanks,

 

John

Attachments:
image
  • Sign in to reply
  • Cancel

Top Replies

  • jw0752
    jw0752 over 6 years ago +5 verified
    Hi John, I recently had a circuit that sensed AC mains using an AC optocoupler. This would allow you to sense the mains without a direct connection to the rest of your circuit. On my board they used a…
  • shabaz
    shabaz over 6 years ago in reply to johninjax +3 suggested
    Hi John, Could you explain your actual goal / use-case? The trouble is, with the small bit of information, any answer may not be appropriate or may not help you, because the answer can be different based…
  • jw0752
    jw0752 over 6 years ago in reply to johninjax +3
    Hi John, You have probably noted that since your latch relay is either one side or the other you really only need to sense one side . If you build a circuit like the one I experimented with it will light…
Parents
  • colporteur
    0 colporteur over 6 years ago

    Well labelling you as crazy is a conjecture at this point. Reducing AC mains to a lower voltage by using a dropping resistor might put you in the running.

     

    I'm not confident I have a full understanding of your circuit. You have a 5VDC powered SPDT latching relay you are going to use/test. You want to tap the AC mains using a dropping resistor, rectify and filter the output to power the relay?

     

    Why not just test the relay contacts for continuity? That can tell you what side is engaged.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • colporteur
    0 colporteur over 6 years ago

    Well labelling you as crazy is a conjecture at this point. Reducing AC mains to a lower voltage by using a dropping resistor might put you in the running.

     

    I'm not confident I have a full understanding of your circuit. You have a 5VDC powered SPDT latching relay you are going to use/test. You want to tap the AC mains using a dropping resistor, rectify and filter the output to power the relay?

     

    Why not just test the relay contacts for continuity? That can tell you what side is engaged.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • johninjax
    0 johninjax over 6 years ago in reply to colporteur

    Added a pic like what I am talking about.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • shabaz
    0 shabaz over 6 years ago in reply to johninjax

    Hi John,

     

    Could you explain your actual goal / use-case?

    The trouble is, with the small bit of information, any answer may not be appropriate or may not help you, because the answer can be different based on context.

    Some example things that can usually help (not all may apply):

    1. My Goal in detail

            (e.g. climb a mountain next year)

    2. What things I'm trying to solve

             (e.g. establish how high I am)

    3. What constraints I have

             (e.g. cost, software experience, hardware experience)

    4. What hardware, tools and software I'm using

             (e.g. part number, link to the tools and software)

    5. Diagram or sketch to show the scenario, and what I've attempted

    6. Where I believe the problem lies, or which part I need help on

              (e.g. unexpected response from the part I'm using)

    7. Non-blurry photographs of the set-up (zoomed out for context, and detail), and video if needed

    Non-fuzzy, focussed Overview Photo (for context)

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • jw0752
    0 jw0752 over 6 years ago in reply to johninjax

    Hi John,

    The picture didn't post. Make sure you use the Icon in the tool bar that looks like  to insert pictures with your text.image

     

    John