Power & Energy
  • Technologies
  • More
Power & Energy
Forum How to sense mains AC?
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 8 replies
  • Answers 2 answers
  • Subscribers 283 subscribers
  • Views 1871 views
  • Users 0 members are here
Related

How to sense mains AC?

johninjax
johninjax over 6 years ago

Hey,

I need to know if a latching SPDT relay is on the A or B side. The relay has a 5V control, but it will have 120VAC on it. I was planning to use a half wave rectifier and RC filter with large R to tap off ~5V into a gate. Am I crazy? Is there a better/simpler way?

 

Thanks,

 

John

Attachments:
image
  • Sign in to reply
  • Cancel

Top Replies

  • jw0752
    jw0752 over 6 years ago +5 verified
    Hi John, I recently had a circuit that sensed AC mains using an AC optocoupler. This would allow you to sense the mains without a direct connection to the rest of your circuit. On my board they used a…
  • shabaz
    shabaz over 6 years ago in reply to johninjax +3 suggested
    Hi John, Could you explain your actual goal / use-case? The trouble is, with the small bit of information, any answer may not be appropriate or may not help you, because the answer can be different based…
  • jw0752
    jw0752 over 6 years ago in reply to johninjax +3
    Hi John, You have probably noted that since your latch relay is either one side or the other you really only need to sense one side . If you build a circuit like the one I experimented with it will light…
Parents
  • dougw
    0 dougw over 6 years ago

    Looks like a pretty hairy way to try to reduce voltage. - not sure why the switch is wired like that.

    I've seen some motor controllers that use a sort of capacitor divider (C-R-C) to supply low voltage to the control circuitry, but it was all self-contained. You wouldn't want to poke around in there expecting to find just low voltage.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • dougw
    0 dougw over 6 years ago

    Looks like a pretty hairy way to try to reduce voltage. - not sure why the switch is wired like that.

    I've seen some motor controllers that use a sort of capacitor divider (C-R-C) to supply low voltage to the control circuitry, but it was all self-contained. You wouldn't want to poke around in there expecting to find just low voltage.