Hi, I am in crisis with an energy harvesting design. I'll try to explain this:
I have 6 solar panels (with about 20V and 1A at maximum power), which receive very different lighting from each other. For example, I can have 1 panel at maximum power, 2 panels at medium power and others in the dark.
I started a design with LT3652 MPPT, but I have a problem: how can I get power from all solar panels, even with different voltages?
If I put all panels in parallel, through 6 diodes, at the input of the MPPT, only the panel with the highest voltage will transfer its power to the MPPT. So, if I have other active panels with a lower voltage, they won't contribute to the system power.
If I use a different MPPT for each panel, I can get the same output voltage from each active panel (with a minimum input voltage threshold). But how can I use 6 different output, with the same voltage, summing the current, at the input of a battery charger (e.g. LT1513)? If I put a diode between each MPPT output and the battery charger input, I think only one regulator will "win" and power the charger. Correct?
Do you have some solution or suggestions?
I've been looking for similar solutions online for days, but without success.
Thanks in advance...
Simone