Power & Energy
  • Technologies
  • More
Power & Energy
Forum Universal charger
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 6 replies
  • Subscribers 283 subscribers
  • Views 955 views
  • Users 0 members are here
  • phones
  • mobile
  • adapter
  • universal
  • power
Related

Universal charger

GardenState
GardenState over 16 years ago
The International Telecommunications Union (ITU) has given its stamp of approval to an energy-efficient, one-charger-fits-all mobile phone solution. Based on the Micro USB interface and called the Universal Charging Solution (UCS) it will enable the same charger to be used for all future handsets, regardless of make and model. Consumers have clamored for a universal charger for years, but is Micro USB the right platform?
  • Sign in to reply
  • Cancel
Parents
  • Former Member
    0 Former Member over 13 years ago

    I never think we will ever get a universal charging platform other than what we have right now with the micro USB other than Apple.  I remember when all these tech was coming out is was a mess but it has cleaned up now.  The problem i see right now, is that every device has a different size battery pack (mAHr) and until you get every device to have the same battery pack, then we can all have the same charger.  I even seen devices have the same battery pack, and the two different company had different rated chargers!  How fast you charge a battery will always be a at the engineer design philosophy and will vary engineer to engineer.  When i design my charging system i charge it at the lowest charge rate as I can as i want to preserve the life of the battery.  Also, usb computer connections are already standardized  across all platforms as the max charge current is 500mA no matter what we plug in.  One thing i love about Li-ion batteries is that all the brains are contained inside the module.  This is due to how toxic Li can be, and thus it contains a temp sensor, battery charge level indicator,  a over charge protection shut off relay, etc...  If building a smart charger for Nicads, the user has the build all these ckt but not so much with Li-ion battery!  Anyways consider that we already have a universal charger right now!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • MikeGreen
    0 MikeGreen over 13 years ago in reply to Former Member

    Hi Eric et al,

    Actually the latest USB battery charging spec allows a range of currents up to 1.8 A to be supported. This means that USB very well placed to become the universal charging interface in future electronic designs. The EU has already made it mandatory for all new smartphone models to include a USB port for charging as well as data purposes. FTDI, one of Element 14 franchised manufacturing partners, has written extensively on this subject. Here is an example if you are interested - http://electronicdesign.com/article/power/usb-spec-improves-charging-portable-devices-73831 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • MikeGreen
    0 MikeGreen over 13 years ago in reply to Former Member

    Hi Eric et al,

    Actually the latest USB battery charging spec allows a range of currents up to 1.8 A to be supported. This means that USB very well placed to become the universal charging interface in future electronic designs. The EU has already made it mandatory for all new smartphone models to include a USB port for charging as well as data purposes. FTDI, one of Element 14 franchised manufacturing partners, has written extensively on this subject. Here is an example if you are interested - http://electronicdesign.com/article/power/usb-spec-improves-charging-portable-devices-73831 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
No Data