Power & Energy
  • Technologies
  • More
Power & Energy
Forum UC3842
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 5 replies
  • Subscribers 283 subscribers
  • Views 1591 views
  • Users 0 members are here
Related

UC3842

e14 Contributor
e14 Contributor over 16 years ago

I like to know how can I make "hi cup" protection on SMPS flyback based on UC3842.

Secondary feedback with TL431 and FB pin is placed to ground.

The COMP pin is pull up with resistor from VREF.

In the COMP pin we connect the optocoupler.

We see from a lot of people place a series resistor from bias to vcc for power supply, is this the solution? make a UVLO?

 

Regards,

 

J.A.M.

  • Sign in to reply
  • Cancel
Parents
  • enrico.migchels
    0 enrico.migchels over 16 years ago

    Hoi Jose,

     

    I don't know exactly what circuit you use but a nice way of making a hiccup mode is to pull the ''Comp'' pin to ground (Vcomp < 1V). You can achieve this by adding a discrete SCR (thyristor, 2 transistor circuit) and sensing on both the auxilairy supply voltage (Vout too high -> Vaux rises too high -> fire scr) and (Vout shorted -> Feedback too low -> fire SCR). You can add an RC-network with a considerable time constant (eg 22uF / 47kOhm) to keep the SCR activated for a long time when fired, resulting in a low hiccup frequency. If the above is to not clear enough i can upload a simplified diagram (if you want).

     

    Best regards,

     

    Enrico Migchels

    Power Conversion Design Engineer

    Heliox B.V.

    Best - The Netherlands

    www.heliox.nl

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to enrico.migchels

    Hello Enrico,

     

    We have some problems with same question. Can you send me part of the schematic for make a real and nice HICUPP when the output is shorted?

     

    Regards,

     

    José Antonio

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to enrico.migchels

    Hello Enrico,

     

    We have some problems with same question. Can you send me part of the schematic for make a real and nice HICUPP when the output is shorted?

     

    Regards,

     

    José Antonio