Power & Energy
  • Technologies
  • More
Power & Energy
Forum Power Switching Device
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 8 replies
  • Answers 1 answer
  • Subscribers 285 subscribers
  • Views 1058 views
  • Users 0 members are here
Related

Power Switching Device

e14 Contributor
e14 Contributor over 16 years ago

Hi Guys,

 

I believe it is my first time posting here as I have finally figured out what question i need to ask.

 

I have a need for an electronic switching device. These are the requirements

 

-> Switching 120VAC (VDS?) on/off

-> Controlling ON voltage: 5V (switched from a microcontroller)

-> Drain-Source Current IDS between 3-5A continous

-> Size wise, small enough to fit on a PCB

 

I am thinking an N-Type MOSFET will work but should I also be looking at BJT's or SCRs? I don't have a lot of practical experience here so any help is appreciated. Let me know if you need more information.

 

Thanks!

 

Duncan

 

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 16 years ago

    I guess you could take a look at IGBTs. They are very easy to control and very resistant. But it depends on what do you need it for...is it a rectifier? I used full-bridge of IGBTs for a rectifier with grid interface, it worked fine!

     

    http://pt.farnell.com/fairchild-semiconductor/fgh50n6s2d/igbt-n-to-247/dp/1095034

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 16 years ago in reply to e14 Contributor

    Hey Pedro, thanks for the reply.

     

    No, this is not a rectifier. The AC would need to pass through the device unmodified (60Hz). It also shouldn't be amplified. I just need it switched on or off.

     

    I didn't actually know about IGBT's until you mentioned them and looked them up. Are they widespread? Do you know where they are used?

     

    See attached, quick sketch of possible configuration of the device. Gate voltage of 5V. Any thoughts?

    Attachments:
    imageschematic2.pdf
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • KennyMillar
    0 KennyMillar over 16 years ago in reply to e14 Contributor

    Many cicuits switch mains loads.

     

    You could use a simple 5V Coil relay such as G5LE (farnell part number 1333640) which easily be switched by 5V (use NPN transistor such as 2N3904 to switch the coil, and protect the circuit with a didode such as 1n4004 reversed across the coil)

     

    You could also use an SSR (solid state relay) such as S21601F (farnell 1618479) - which gives a very neat solution - you must add a snubber circuit (Resistor + Capacitor) to prevent accidental switching.

     

    Note that this SSR requires a control current of 50ma, so don't drive it direct from a processor pin, again use something like an NPN transistor to switch it.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 16 years ago in reply to KennyMillar

    Thanks Kenny.

     

    The coil sounds like a good idea. Since it is simple, I could probably start there and try another method if I am successful. Just wondering, how does placing a dioide across the coil protect the circuit? I drew a simple circuit. Does it look right?

     

    A Triac sounds like it could also do the trick, and as you mentioned would probably need a transistor for the higher gate current capabilities.

     

    Thanks for your input.

     

    Duncan

    Attachments:
    imageSchematic3.pdf
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • KennyMillar
    0 KennyMillar over 16 years ago in reply to e14 Contributor

    The circuit is pretty much ok, but I'd probably use a small series resitor inline with the base of the transistor, say 820 Ohm.

     

    Current flowing through a relay coil creates a magnetic field which collapses suddenly when the relay is switched off. This sudden collapse of the magnetic field induces a brief high voltage across the relay coil. The diode feeds the current back through the coil (and diode) so the magnetic field dies away over a short time rather than instantly. This prevents the induced voltage becoming high enough to cause damage.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 16 years ago in reply to KennyMillar

    Yeah, I think there needs to be that series, gate resistor present. Not sure why I didn't include it. image

     

    Ok I see how it works. I have seen the diode present in motor control devices and wasn't quite sure the use for it. (Of course motors are just inductive loads.)

     

    I realize now that the switching frequency of the relay may be up to 10Hz so that might be a little fast for a mechanical switch. In this case a SSR would work (using a Triac). I plan on testing the circuit at a lower frequency, 1Hz, so I will still likely try using the mechanical relay first.

     

    Thanks for the input.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 16 years ago in reply to KennyMillar

    Yeah, I think there needs to be that series, gate resistor present. Not sure why I didn't include it. image

     

    Ok I see how it works. I have seen the diode present in motor control devices and wasn't quite sure the use for it. (Of course motors are just inductive loads.)

     

    I realize now that the switching frequency of the relay may be up to 10Hz so that might be a little fast for a mechanical switch. In this case a SSR would work (using a Triac). I plan on testing the circuit at a lower frequency, 1Hz, so I will still likely try using the mechanical relay first.

     

    Thanks for the input.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 16 years ago in reply to e14 Contributor

    Think you are looking for a Solid State Relay.

    A while ago i found one with 3 - 9Vdc control voltage.

    Just search it on the net.

     

    Rick

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • francovecchi
    0 francovecchi over 16 years ago in reply to e14 Contributor

    Some time ago I uset a optotriac. It is like a optoinsulator, but with a small triac in output. You can use this small triac to drive a more powerful triac. Two components, optoinsulation and a drive current of few milliamps..... Zero corossing for the less noise.

     

    Regards.

    Franco Vecchi