Power & Energy
  • Technologies
  • More
Power & Energy
Forum Triple rail power supply design
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 3 replies
  • Answers 1 answer
  • Subscribers 282 subscribers
  • Views 816 views
  • Users 0 members are here
  • ac-dc
Related

Triple rail power supply design

e14 Contributor
e14 Contributor over 16 years ago

Hi, I have a need for a power supply that can deliver +5 @7A min ,-5@7A min and +12v@ >1A min with as little noise as possible , the source is standard 230v@50hz. There has allready been two different designs, the first one used switching psu:s but the output was not good enough (too much noise etc.).

     The second one uses Power-One HN5-9/OVP-A x2 and HB12-1.7 x1 Linear psu:s. These work very well but I would like some alternatives to possibly increase the output power with pretty similar device footprint, those HN5 are pretty much as large as I can fit to the case I am using and seem to have been discontinued from farnell catalog. So would a large power switching supply with some sort of efective regulation and noise filtering be the better choice when considering size/price etc. Also what kind of filtering would be efective with the switching supplies, I allready have few of the old versions so they could propably work with some sort of filtering/stabilization circuitry.

  • Sign in to reply
  • Cancel
Parents
  • enrico.migchels
    0 enrico.migchels over 16 years ago

    Hi there Antto,

     

    I don't know what your ripple and noise demands are, but if they are in the mV-range you could buy 3 SMPS products (2 x 5V, 1 x 12V) and improve the output stage. Start by replacing the output capacitors of the power supplies by really good onces. The main parameter to look for is ESR, the series impedance of a capacitor is the cause for ripple, the ESL is often the cause for the noise. To give you some insight in good capacitors: Supplier NCC, series KZH. If the improvement in ripple and noise is not sufficient, add a second filtering stage after the power supply. Build a 2-orde filter = series coil and after that: capacitor to ground. The inductance should be as high as possible but this is difficult when the current is 7A. A few mH should be no problem. Don't use a common mode choke but a drum core or even a transformer bobbin with a gapped ferrite core. use thick wires to avoid voltage loss across the coil. To damp the noise spikes you can also add ferrite beads (with multiple turns) in series with the outputs.

     

    Best regards,

     

    Enrico Migchels

    Power conversion design engineer

    Heliox B.V.

    Best - The Netherlands

    www.heliox.nl

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • enrico.migchels
    0 enrico.migchels over 16 years ago

    Hi there Antto,

     

    I don't know what your ripple and noise demands are, but if they are in the mV-range you could buy 3 SMPS products (2 x 5V, 1 x 12V) and improve the output stage. Start by replacing the output capacitors of the power supplies by really good onces. The main parameter to look for is ESR, the series impedance of a capacitor is the cause for ripple, the ESL is often the cause for the noise. To give you some insight in good capacitors: Supplier NCC, series KZH. If the improvement in ripple and noise is not sufficient, add a second filtering stage after the power supply. Build a 2-orde filter = series coil and after that: capacitor to ground. The inductance should be as high as possible but this is difficult when the current is 7A. A few mH should be no problem. Don't use a common mode choke but a drum core or even a transformer bobbin with a gapped ferrite core. use thick wires to avoid voltage loss across the coil. To damp the noise spikes you can also add ferrite beads (with multiple turns) in series with the outputs.

     

    Best regards,

     

    Enrico Migchels

    Power conversion design engineer

    Heliox B.V.

    Best - The Netherlands

    www.heliox.nl

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 16 years ago in reply to enrico.migchels
    Thanks for the tips, I will check the older designs and will try to improve on them. The SMPS would be nice in the power/size ratio because the current suplies are allready under fairly high load. Do you happen to have any suggestion on SMPS manufacturers with good units in reasonable prizerange.
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • enrico.migchels
    0 enrico.migchels over 16 years ago in reply to e14 Contributor

    Hi Antto,

     

    I build custom power supplies for customers with specfic requirements. If the number of products/year is high enough you could decide to have a custom design. If i would have to select a standard off-the-shelve power brick i would make a short list of demands and try to find a fit at a large distributer, like Farnell. Availability is also a key parameter.

     

    Best regards,

     

    Enrico Migchels

    Power Conversion Design Engineer

    Heliox B.V.

    Best - The Netherlands

    www.heliox.nl