Power & Energy
  • Technologies
  • More
Power & Energy
Forum NPN & PNP matched pairs at 10A
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 6 replies
  • Subscribers 282 subscribers
  • Views 1214 views
  • Users 0 members are here
  • dc-dc
  • signal
  • management
  • power_management
  • power
Related

NPN & PNP matched pairs at 10A

Catwell
Catwell over 16 years ago
This is a major issue I've been having lately. I am designing H-Bridges for stepper motors. And at low amperage, 2A -5A, matching resistance of the NPN and PNP Mosfets is easy, having a perfectly balance bridge. But when you get into the 10A range, that is where the matching ends. What I find is that almost always the PNP has a higher resistance than the NPN.
 
I know there are ICs that are complete H-bridges, but I haven't found any that can handle 10A or more. So, I am going to stick with building the bridge from individual Mosfet.
 
With that being said, where can I find impedance matched NPN and PNP pairs that can handle 10A or more? Any help would be greatly appreciated.
 
Cabe
  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 16 years ago

    I assume by PNP/NPN you mean N channel & P channel mosfets here?

     

    Why do you want them matched? What does it matter if the bridge is not "perfectly balanced"?

     

    R

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • albertosombri
    0 albertosombri over 16 years ago in reply to e14 Contributor

    PNP/NPN doesn't mean Mosfet N or P channel, but means NPN BJT and PNP BJT there are many difference in between.

    Well balanced bridge it's necessary in order to balance the power dissipation on those devices.

     

    I believe you have to use a complementary devices, just like used in audio power amplifier.

    I will check on one of my audio amplifier built many years ago, if I remember well the power BJT were MJE series.

     

     

    Regards

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 16 years ago in reply to albertosombri

    Yeah but why does the bridge have to be "balanced". Anyway to use Mosfets instead of BJT is a better idea esp at higher voltages in my opinion, I've had enough of second beakdown..

     

    R

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 16 years ago in reply to albertosombri

    Yeah but why does the bridge have to be "balanced". Anyway to use Mosfets instead of BJT is a better idea esp at higher voltages in my opinion, I've had enough of second beakdown..

     

    R