Power & Energy
  • Technologies
  • More
Power & Energy
Forum Recommendation for DC to DC circuit ??
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 284 subscribers
  • Views 305 views
  • Users 0 members are here
Related

Recommendation for DC to DC circuit ??

Former Member
Former Member over 15 years ago

Looking for a recommendation for a simple DC to DC converter - preferred one chip solution  - not BGA

Input approx.  24 VDC

Dual output  :   plus +12 VDC  and minus -12 VDC   ( +12V to GND and -12V to GND)

Current  approx  0.5A  to  1A

  • Sign in to reply
  • Cancel
Parents
  • ksmith
    0 ksmith over 15 years ago

    Werner,

     

    XP Power has many different choices that could be used as a single part solution.

     

    It will heavily depend on whether you want 0.5A or 1A on each of the 12V rails, or some value in between as we have many different solutions from 12-25W of power.

     

    Some options to begin looking at would be the JTF12, JTK15, JCK15, JCK20, JCK30.

     

    There are still further options that you could look at via our website at www.xppower.com, or you could contact one of our sales offices to discuss it further with a sales person.

     

    Thanks,

     

    Kent Smith

    XP Power

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 15 years ago in reply to ksmith

    hI

      Thank you for the information , but I was more thinking on a circuit ic , to be mounted on the pcb , with a inductor and some components around

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Former Member
    0 Former Member over 15 years ago in reply to ksmith

    hI

      Thank you for the information , but I was more thinking on a circuit ic , to be mounted on the pcb , with a inductor and some components around