Power & Energy
  • Technologies
  • More
Power & Energy
Forum Tireless search for a small 5A H-Bridge
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 9 replies
  • Subscribers 286 subscribers
  • Views 1361 views
  • Users 0 members are here
  • stepper_motor
  • power_management
  • cnc
  • power_supply
  • power
  • servo_motor
Related

Tireless search for a small 5A H-Bridge

Catwell
Catwell over 16 years ago
I need a small H-bridge option, similar to this Maxim 1A H-Bridge IC, but could handle at least 4A, ideally 5A. It doesn't have to be in a 8-SOIC package, but I do not want a 2"x2" PCB version either. A single chip would be best.
 
Thoughts?
 
This will be for a stepper/servo motor driver, ultimately.
 
Cabe
  • Sign in to reply
  • Cancel
Parents
  • ChuckMcM
    0 ChuckMcM over 13 years ago

    Ok, 5A for a full bridge isn't going to be easy to find in a single chip. You're looking at i2r losses of 5W for .1 ohm fets and 500mW for .01 ohm fets That means you are looking at D9 packages at the minimum for discrete FETs (no SOT23's will carry that much current and not desolder themselves). The typical TO-220AB package will dissipate 2.5W in free air. I wrote up a tutorial on h-bridges here http://www.mcmanis.com/chuck/robotics/tutorial/h-bridge/index.html and will follow up with a FET version here now that I've got stuff worked out on the web site (new site will be http://robotics.mcmanis.com)

     

    The way to look at this is what the Rds(on) value is for the FET, then square the current and multiply that by 2 (high side fet and low side fet) that is the power that has to be dissipated by the package. If the temperature goes up (which it will do without a heat sink) then Rds goes up too (which means more power gets dissipated) Good general rule of thumb is that Rds(on) doubles at max temperature. So if the data sheet says it has a 1 milliohm Rds(on) then at full temp that will be 2 milliohms. On steppers you probably want a good chopper drive anyway to get maximum torque out of them.

     

    ---Chuck

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • ChuckMcM
    0 ChuckMcM over 13 years ago

    Ok, 5A for a full bridge isn't going to be easy to find in a single chip. You're looking at i2r losses of 5W for .1 ohm fets and 500mW for .01 ohm fets That means you are looking at D9 packages at the minimum for discrete FETs (no SOT23's will carry that much current and not desolder themselves). The typical TO-220AB package will dissipate 2.5W in free air. I wrote up a tutorial on h-bridges here http://www.mcmanis.com/chuck/robotics/tutorial/h-bridge/index.html and will follow up with a FET version here now that I've got stuff worked out on the web site (new site will be http://robotics.mcmanis.com)

     

    The way to look at this is what the Rds(on) value is for the FET, then square the current and multiply that by 2 (high side fet and low side fet) that is the power that has to be dissipated by the package. If the temperature goes up (which it will do without a heat sink) then Rds goes up too (which means more power gets dissipated) Good general rule of thumb is that Rds(on) doubles at max temperature. So if the data sheet says it has a 1 milliohm Rds(on) then at full temp that will be 2 milliohms. On steppers you probably want a good chopper drive anyway to get maximum torque out of them.

     

    ---Chuck

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to ChuckMcM

    I cant see the required Vds for the MOSFETs but here are a few options from FSC that at least provide the full bridge set of FETs in one small package although Rds(on) might be a bit high on the 100Vds parts

     

    Quad MOSFET package

    FDMQ8203- 100Vds 2( Nch + Pch) MOSFET for full bridge

    FD/FDMQ8403- 100Vds 4* Nch MOSFET

    FDMQ86530L- 60Vds 4* Nch MOSFET (logic level switching)

     

    LV Bridge Drivers

    FAN3268 20V bridge driver

    FAN3278- 30V bridge driver