Power & Energy
  • Technologies
  • More
Power & Energy
Forum Ferrite for GND separation
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 4 replies
  • Subscribers 284 subscribers
  • Views 1374 views
  • Users 0 members are here
  • linear
  • power_management
  • filtering
  • power_distribution
  • isolation
  • ferrite
  • power
  • filter
Related

Ferrite for GND separation

Former Member
Former Member over 15 years ago

Hi

 

I need to create a few low disturbance voltages  to use with a analog video decoder. I need one 3.3V for digital  circuitry, one 3.3V for analog, one 1.8V for digital and one 1.8V to  drive a PLL. I want thous voltages to have separate GND from the rest  of the circuit, one for digital and one for analog circuitry.

I believe it will be sufficient to use ferrite beads to "isolate" these  voltages from the main voltage and GND, but I'm not sure which  characteristics the ferrite beads need to have.

There are no particular frequencies that I'm aware that I need to  filter. The main 5V is created from a 850KHz DC/DC step down switcher  though.

I'm not sure about the current consumption of the four voltages, but it  can be assumed to be less than 40mA each, and less than 100mA in total.

Price is a factor of course, but also the size is fairly important. I would also much prefer SMD components.

I guess I need fairly low impedance components, but otherwise I'm not sure what to look for.

Does anyone have any components to recommend, or at least some general hints? All help is much appreciated.

 

Kind regards

Albin, Sweden

Attachments:
image
  • Sign in to reply
  • Cancel
Parents
  • lfa555
    0 lfa555 over 15 years ago

    Dear Afbin,

     

    thanks a lot for posting the question.

     

    As you already mentioned a chip beat ferrite might be here your best solution since the parts are fairly in expensive with a high level of EMI noise rejection (in differantial mode).

     

    For small DC/DC Converter applications we recommend our WE-CBF Wide Band series:

    http://katalog.we-online.de/kataloge/eisos/index.php?language=xx&pf=WE-CBF

     

    The Wide Band series has the advantage of suppressing EMI noise on a broad frequency spectrum. They all full fill your current requirement and are effective in combination with your dcdc swithcing frequency.

     

    Then it is all depending in which frequeny band you see spikes to make the right selection. Our recommendation is in this case to make some test with different components out of our WE-CBF 0603 or 0805 Wide Band series.

    Instead of buying all components separately the optimum for you would be to get our Chip Beat assortment with the full band of values in 0805, 0603 and 0402 sizes to find the best component for the applcation. The part number is 742790.

     

    I will have Farnell make the kit also available on the web the next days. If there is a need of the kit the next 2-3 days you can either buy a selection of the components or you can also order the kit directly at www.we-online.de

     

    If you have any request please let me know.

     

    regards

    Lars Fahrbach

     

    Würth Elektronik

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 15 years ago in reply to lfa555

    Thank you Lars!

     

    I'll choose one or two ferrites from the WE-CBF series to begin with and order a design kit when the need to tweak the filtration.

     

    Kind regards

    Albin, Sweden

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Former Member
    0 Former Member over 15 years ago in reply to lfa555

    Thank you Lars!

     

    I'll choose one or two ferrites from the WE-CBF series to begin with and order a design kit when the need to tweak the filtration.

     

    Kind regards

    Albin, Sweden

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
No Data