Power & Energy
  • Technologies
  • More
Power & Energy
Forum Transformers VT relationship with error?
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 3 replies
  • Subscribers 283 subscribers
  • Views 600 views
  • Users 0 members are here
Related

Transformers VT relationship with error?

Eavesdropper
Eavesdropper over 15 years ago

In a transformer I apply a low percentage of the rated primary voltage and get a secondary output of the primary divided by the VT ratio. On many transformers this doesn't hold true, and I get errors over 15%. However, when applying higher voltages, the error isn't noticeable. Can someone explain the relation of VT and error?

Thanks.

E

 

  • Sign in to reply
  • Cancel
Parents
  • jvdberg@ieee.org
    0 jvdberg@ieee.org over 15 years ago
    What you noticed is not an error.
    In transformers there are losses, due to the ohmic resistance of the wire.
    (there are also magnetic losses)
    To meet the specifications, the ratio of turns is not equal to the ratio of the voltages.
    When loaded with a resistive load at the specified voltage and current, the voltage ratio will meet the label values.
     
    At a low output current, the secondary voltage will be higher.
    With a pulsed load, like a bridge rectifier and capacitor, the secondary voltage will be lower.
     
    For calculations a transformer will act as an ideal transformer with a resistor in series.
     
    Very small transformers and small transformers with an extra isolation between primary and secondary have more losses than big transformers.
    In small transformers a relative large amount of available space in the core is used for insulation. So thinner wire must be used to fit into the available space.
    Small transformers have a big surface relative to their power so they can easily dissipate the heat caused by the losses.
     

    When a transformer is used at a much lower voltage than rated, those losses are higher than necessary. A lower number of turns could have been used, leaving space to use thicker wire

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • Eavesdropper
    0 Eavesdropper over 15 years ago in reply to jvdberg@ieee.org

    JV,

     

    Thank you for the explanation. So, the transformers are wound to meet minimum specs? That means they come with built in errors and inefficiencies. What a disappointment. Can you recommend further reading on the subject?

     

    E

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Eavesdropper
    0 Eavesdropper over 15 years ago in reply to jvdberg@ieee.org

    JV,

     

    Thank you for the explanation. So, the transformers are wound to meet minimum specs? That means they come with built in errors and inefficiencies. What a disappointment. Can you recommend further reading on the subject?

     

    E

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • jvdberg@ieee.org
    0 jvdberg@ieee.org over 15 years ago in reply to Eavesdropper

    Unfortunately most devices are not ideal. For further reading I saw an easy to understand artcle at http://en.wikipedia.org/wiki/Transformer

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer