Power & Energy
  • Technologies
  • More
Power & Energy
Forum Inrush current limit
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 14 replies
  • Answers 2 answers
  • Subscribers 285 subscribers
  • Views 4307 views
  • Users 0 members are here
  • inrush
  • circuit
  • protection
  • power
Related

Inrush current limit

ZeroSizeObject
ZeroSizeObject over 15 years ago
I have a  circuit that runs at 5V ~200mA. When the system in turned on I get a spike of about 2A. Repeated cycling will kill the core circuit.
 
What are some strategies to protect my circuit?
 
Zero
  • Sign in to reply
  • Cancel
  • DAB
    0 DAB over 15 years ago

    Use ferrite beads over the wires, they create an inductance reactance that slows the current surge.

    Thanks

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • ZeroSizeObject
    0 ZeroSizeObject over 15 years ago in reply to DAB

    That would be one big ferrite bead. What if the current frequency is very high, doesn't a bead have a limit to what it can suppress?

     

    Zero

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 15 years ago in reply to ZeroSizeObject

    2A Beads are available over a wide frequency/current range and sizes(like even in 0402 package) i believe.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • DAB
    0 DAB over 15 years ago in reply to ZeroSizeObject

    Take a look at what type of bead they use in your PC's power supply.  Another good source is the old CRT monitors, they usually had a fairly large bead to keep the HF from getting back to the power supply.

    I am not an expert on the beads, but I have been involved in projects where we needed to cut down on the inrush currents and the engineers I worked with used the beads effectively.

    Hopefully this points you in the right direction.

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • ZeroSizeObject
    0 ZeroSizeObject over 15 years ago in reply to DAB

    Dab,

     

    Thanks, I will look into it more.

     

    Zero

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 15 years ago

    If the inrush if from large capacistors in the circut, ferrit beeds does  not help you - you will need a larger inductor to do the jobb then, but  it is better done with a mosfet as a current limiter.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 15 years ago

    Agree with Bengt Rehnström. ferrit bead can't help. you need some resistance, not inductance.

    In the PC power supply, the bead core on the wire is for noise filter.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 15 years ago in reply to e14 Contributor

    Some good reading:

    http://www.eet-china.com/ARTICLES/2000DEC/2000DEC13_AMD_AN5.PDF?SOURCES=DOWNLOAD

    Or just seash for "an1542" it is a more or less standard AN to read.

     

    I have used inductiv, fixed value resistors, NTC and active MOSFET controll i designs in order to keep the inrush under controll - With EUP and for mbattery powered equipment it is not an option to use the NTC because it lowers the system over all effinency. One other option that is usefull in some situations is the PROFET from INFINEON - you have to check there datasheet - they have serveral different for different applications.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 15 years ago in reply to e14 Contributor

    I have used some hot-swap control methods in my designs which does similiar functions like inrush/over current limiting....... which is same as mentioned in the article like soft turn on of a MOSFET.....

     

    The inrush current is largely depends on the value of the bulk capacitor on the supply input(like dc-dc converter input cap) which are used as a temporary storage and it's value largely varies with the input voltage range.....

     

    its always better to use the active control method such as turning on a MOSFET slowly initially to avoid the initial inrush.......but in this case, considering such solutions costly i would suggest to add an inductor in series with the input capacitor.......

     

    NTC is also a good option since its available even in 20mohms at max current now but it can be a little bulky.......selection largely depends on what resistance value is required during the turn-on time(or what current to be limited).....

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 15 years ago in reply to e14 Contributor

    Hi, check out the FPF2123FPF2123 from Fairchild Semiconductor, its a load switch with programmable overcurrent limit, it will operate at constant current when the (programmable) limit is reached, otherwise it will just turn fully on. should solve your problem!

    Let us know if that worked...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
>