Power & Energy
  • Technologies
  • More
Power & Energy
Forum NECULEAR ENERGY-TO POWER A POPSICLE MACHINE
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 0 replies
  • Subscribers 282 subscribers
  • Views 273 views
  • Users 0 members are here
  • Alternative Energy Tags
  • innovation
Related

NECULEAR ENERGY-TO POWER A POPSICLE MACHINE

e14 Contributor
e14 Contributor over 15 years ago

So well lets start a discussion, What do ya  think. Sorta about stuff. So what's knew, same old lets do lets don't. Sure it can be done. Make Popsicles, for real, useing neclear energy. Ya but how?  The little buggers will melt, likely before we even realize our dream. I have read in another discussion that some very astute individuals are in the process of creating a thingie thing that takes pot shots at little beads, sure nothing wrong with that, if one likes shooting at little glass beads, not for sure knowing the consequence of such as is this activity. Well, to boil water, if that is the goal, likely will turn the steam into vapor before it can be utilized for such a worthy purpose. And as well, such a project, as to produce enough energy on a constant basis, not knowing the full outcome, lies within the mindset of speculation. But whooooa, to create a mini sun, wweelllll, that is for sure within the realm of speculation. I thought only the creator, created stuff like that. A six million degree temperature from taking pot shot at gass little bead things, is truth positive the creator may want to look into it. Perhaps their is an investment forthcoming, like bricks and stuff, that can be used for cooling, like they use on the shuttle space thing. But as it is, hope that all goes well with the venture. You may want to browse the topic as it is in another discussion. Most interesting stuff. But sure, neclear energy has it's place, as it is most abundant. however, I for one do not at all feel that it is being used wisely. It is indeed possible, to create the reaction necessary to produce energy, from nuclear particles. And but of course without the enormous heat. But to create a sun, would be asking a bit too much, from what we well know cannot be contained, as we have so proven. If we were to eliminate the enormous heat, reduce the amount of radiation, contain  the ultraviolet radiation, bring forth a reduction of the electromagnetics, as well, place the index on a scale of kelvin, instead of F, we could make popsicles instead of bombs, and the wide spread of a bunch of bad stuff that makes us sick, well, it would just sorta go away. That is, as we enjoy a new environment. And but for the sustainment of such as is this minipulation of atomic structure, as it is capable of produceing an efficient  amount of energy, as per it's purpose, it is as well capable of it's own efficiency, as it so has been proven.....CONTINUED