Power & Energy
  • Technologies
  • More
Power & Energy
Forum Short Circuit and Reverse Polarity Protection
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 284 subscribers
  • Views 1956 views
  • Users 0 members are here
Related

Short Circuit and Reverse Polarity Protection

jeremyvnc
jeremyvnc over 15 years ago

Can anyone help me?  I have been designing some battery powered circuits and want to add Short Circuit and Reverse Polarity Protection to the boards in case my users put the batteries in wrong and was wondering what were the accepted methods (schematics) to go about adding this level of protection.  I would like it all to be passive components but if someone knows of an ic that does it, please tell me.  My circuits run off of a 9V-12V battery and as low as 3.6V.  Current draw measured at 120mA under normal load but rated to hit as much as 7A under maximum load.

 

Any help/suggestions would be greatly appreciated.

-Jeremy

  • Sign in to reply
  • Cancel
Parents
  • jvdberg@ieee.org
    0 jvdberg@ieee.org over 15 years ago

    A series diode will protect against reverse polarity, however this will lower the battery Voltage by 0.6 Volt. A fuse and parallel (zener)diode will protect against reverse polarity but will blow a fuse if the batteries are inserted the wrong way. If a PPTC resettable fuse is used in combination with a parallel zenerdiode, the circuit is protected against reverse polarity, overvoltage and short circuits. The PPTC resettable fuse will disconnect the circuit if the batteries are inserted the wrong way. If the batteries are removed, the fuse will reset. See  http://www.farnell.com/datasheets/612670.pdf  or the farnell catalog for data about PPTC resettable fuses. Johan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • jvdberg@ieee.org
    0 jvdberg@ieee.org over 15 years ago

    A series diode will protect against reverse polarity, however this will lower the battery Voltage by 0.6 Volt. A fuse and parallel (zener)diode will protect against reverse polarity but will blow a fuse if the batteries are inserted the wrong way. If a PPTC resettable fuse is used in combination with a parallel zenerdiode, the circuit is protected against reverse polarity, overvoltage and short circuits. The PPTC resettable fuse will disconnect the circuit if the batteries are inserted the wrong way. If the batteries are removed, the fuse will reset. See  http://www.farnell.com/datasheets/612670.pdf  or the farnell catalog for data about PPTC resettable fuses. Johan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 15 years ago in reply to jvdberg@ieee.org

    You could also use a Schottky diode as a series diode, that will only eat up 0.4V or less (depending on the size of the diode, and the current). Consider the MBR0520L from Fairchild, in a very small package (SOD123) and it has 250mV of voltage drop at room temp and 100mA. A resettable fuse certainly sounds like a good idea

    hope that helps