Power & Energy
  • Technologies
  • More
Power & Energy
Forum Low ESR inductor -> what's the max value?
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 3 replies
  • Answers 1 answer
  • Subscribers 284 subscribers
  • Views 1686 views
  • Users 0 members are here
Related

Low ESR inductor -> what's the max value?

e14 Contributor
e14 Contributor over 14 years ago

Hi,

 

I've started looking into smps some time ago out of curiosity.

Just about everywhere it's mentioned that the inductors used should be "low ESR", but how much is that supposed to be?

I'm looking to buy a basic set of inductors to have around when trying things out, what's a reasonable value to look for?

What's the maximum?

Any good advice on a good starterset is welcome as well ofcourse...

 

Thanks!

 

Dieter

  • Sign in to reply
  • Cancel
Parents
  • Catwell
    0 Catwell over 14 years ago

    Having a set of inductors could be useful, but it may be difficult to pick what range of values you will need. That all depends on the application.

     

    What Vout do you need?

     

    Despite the Vin, the drop across the inductor is typically expressed by V=L*dl/dT

    L = inductance

    dl/dT = rate of change of the current through the inductor. Related to the limits of Iripple

    Always check the current at which the inductor core saturates, this value has to be higher than the applications peak current:  Ipk = Iout +Iripple/2

     

    This should help in deciding based on the application.

     

    Cabe

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • Catwell
    0 Catwell over 14 years ago

    Having a set of inductors could be useful, but it may be difficult to pick what range of values you will need. That all depends on the application.

     

    What Vout do you need?

     

    Despite the Vin, the drop across the inductor is typically expressed by V=L*dl/dT

    L = inductance

    dl/dT = rate of change of the current through the inductor. Related to the limits of Iripple

    Always check the current at which the inductor core saturates, this value has to be higher than the applications peak current:  Ipk = Iout +Iripple/2

     

    This should help in deciding based on the application.

     

    Cabe

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to Catwell

    Thanks!

    And what kind of values am I looking for regarding Rdc (which is the same as ESR I think, no?).

     

    I learned a lot from an EEVblog episode about the MC34063: http://www.eevblog.com/2010/09/10/eevblog-110-lets-design-a-dc-to-dc-switchmode-converter/

     

    Dieter

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • michaelkellett
    0 michaelkellett over 14 years ago in reply to e14 Contributor

    Hello Dieter,

     

    Keeping a set of inductors is even more tricky than resistors or capacitors. There may be some types commonly used in your line of work but the range is so vast that my favourite set would be very different. The way I build up stocks of such parts is buy buying a few extra on each job - that way you accumulate the kind of parts you are likely to want.

    Low series resitance depends on you application - a 1uH inductor for a power supply might have a series resistance of 200mR but so would dissipate 200mW at 1A and I would be happy with it for the power supply of a little audio recorder. If I need 20A then the 80W in the inductor would be aproblem ! Low ESR depends on you application - check specs and remember that the average DC current is what matters for heating but the peak current is what matters for saturation.

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer