Power & Energy
  • Technologies
  • More
Power & Energy
Forum Is there any way a battery can charge other battery through isolated Charging circuit powered by a battery?
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 29 replies
  • Answers 6 answers
  • Subscribers 289 subscribers
  • Views 15364 views
  • Users 0 members are here
  • alternative_energy
  • energy_power
  • energy_storage
Related

Is there any way a battery can charge other battery through isolated Charging circuit powered by a battery?

e14 Contributor
e14 Contributor over 14 years ago

Hi all,

I am just thinking about developing a circuit to charged a 12 Volt battery and the charging circuit will be porwered by a second battery

  • Sign in to reply
  • Cancel

Top Replies

  • kkazem
    kkazem over 14 years ago +2 suggested
    Hi Uche, I'm a master power electronics engineer and I specialize in DC-DC converters, solar charge converters, DC-AC Inverters, Power Supplies, and battery chargers. Yes, you can charge a battery from…
  • YT2095
    YT2095 over 14 years ago +1 suggested
    a battery charger doesn`t care Where it gets its power from, be it mains, solar or another battery, as long as it`s capable of supplying enough power, a regulator can be made to charge a battery from such…
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to YT2095 +1
    Thanks YT2095, I am thinking of developing a power supply that will work for a very long time if not forever when the components are capable of working forever, the system will involve 2x 12 volts batteries…
Parents
  • kkazem
    0 kkazem over 14 years ago

    Hi Uche,

     

    I'm a master power electronics engineer and I specialize in DC-DC converters, solar charge converters, DC-AC Inverters, Power Supplies, and battery chargers. Yes, you can charge a battery from another battery, if that's what you're asking. I don't know why you need it isolated. However, I've got to agree with D2113F with reference to your other replies to this post. To me, it sounds like a perpetual motion machine wheras you have two batteries that are each connected to relays that can switch the individual batteries to either a load or to a a charging circuit fed by the other battery. Here is the problem. Battery-1 is connected to a load and is discharged to the point that you want to rechage it from the other battery that's been idle. Battery-2 recharges Battery-1 thru a dc-dc converter with a control to ensure that it's not overcharged. Now, Battery-2 is discharged and Battery-1 is charged, therefore, the relay or relays setup the circuit such that Battery-1 recharges Battery-2 and now Battery-1 is again discharged. Hopefully, you see where I'm going with this. It's an (almost) endless loop of the batteries charging and discharging each other. And if you powered a load first, discharging Battery-1, then recharged it with Battery-2, Battery-2 is now discharged and you can power the load only one more time with Battery-1. But now, you can no longer recharge Battery-1 with Battery-2 since Battery-2 is discharged, The only way around this is if you have some additional power from another Battery, or a Solar Cell, or from an AC-DC Power Supply to put the lost energy back into the system.

     

    One of the first things you should have learned in physics is that there is no such thing as a perpetual motion machine. Since you used the energy in Battery-1 to power the load and the energy in Battery-2 to recharge Battery-1, and since you used-up the energy in Battery-1 again powering the load after the recharge, you are out of energy as both Battery-1 and Battery-2 are discharged. Does this make any sense to you? I hope so, but if not, please feel free to reply here or send me a message using the Element-14 internal messaging system.

     

    Best regards,

    Kamran Kazem

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • mayavadi
    0 mayavadi over 9 years ago in reply to kkazem

    What about if the other power source is a third battery on the same circuit?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • kkazem
    0 kkazem over 9 years ago in reply to mayavadi

    It doesn't matter if the other power source is a 3rd battery on the same circuit. This kind of cross charging can be done and it will work. What it won't do, however, is to make a perpetual motion or free energy or over unity situation. There are few situations that will even theoretically work that way. One is LENR (low energy nuclear reaction) and another is energy harvesting from existing mechanical, electrical, or thermal energy sources. Like using ocean wave energy to generate electricity or using geothermal energy or wind energy to turn a generator and make electricity. Another example is capturing electromagnetic energy (RF) in wireless form to generate electrical power and this is easily done, but not very practical unless one is near a high-power radio station or HV power line. This is not perpetual motion and it does not violate the laws of physics. It's simply a conversion of one form of energy to another, usually using some excess or easily available energy source. Unless the laws of physics change, nobody will ever take a separate motor and generator, and use the motor to turn the generator to charge the battery that powers the motor to get free, over unity energy. The best one can do in that situation, is to extend the time the motor will run till the battery goes dead for a given apparatus.  

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • kkazem
    0 kkazem over 9 years ago in reply to mayavadi

    It doesn't matter if the other power source is a 3rd battery on the same circuit. This kind of cross charging can be done and it will work. What it won't do, however, is to make a perpetual motion or free energy or over unity situation. There are few situations that will even theoretically work that way. One is LENR (low energy nuclear reaction) and another is energy harvesting from existing mechanical, electrical, or thermal energy sources. Like using ocean wave energy to generate electricity or using geothermal energy or wind energy to turn a generator and make electricity. Another example is capturing electromagnetic energy (RF) in wireless form to generate electrical power and this is easily done, but not very practical unless one is near a high-power radio station or HV power line. This is not perpetual motion and it does not violate the laws of physics. It's simply a conversion of one form of energy to another, usually using some excess or easily available energy source. Unless the laws of physics change, nobody will ever take a separate motor and generator, and use the motor to turn the generator to charge the battery that powers the motor to get free, over unity energy. The best one can do in that situation, is to extend the time the motor will run till the battery goes dead for a given apparatus.