Power & Energy
  • Technologies
  • More
Power & Energy
Forum Is there any way a battery can charge other battery through isolated Charging circuit powered by a battery?
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 29 replies
  • Answers 6 answers
  • Subscribers 289 subscribers
  • Views 15354 views
  • Users 0 members are here
  • alternative_energy
  • energy_power
  • energy_storage
Related

Is there any way a battery can charge other battery through isolated Charging circuit powered by a battery?

e14 Contributor
e14 Contributor over 14 years ago

Hi all,

I am just thinking about developing a circuit to charged a 12 Volt battery and the charging circuit will be porwered by a second battery

  • Sign in to reply
  • Cancel

Top Replies

  • kkazem
    kkazem over 14 years ago +2 suggested
    Hi Uche, I'm a master power electronics engineer and I specialize in DC-DC converters, solar charge converters, DC-AC Inverters, Power Supplies, and battery chargers. Yes, you can charge a battery from…
  • YT2095
    YT2095 over 14 years ago +1 suggested
    a battery charger doesn`t care Where it gets its power from, be it mains, solar or another battery, as long as it`s capable of supplying enough power, a regulator can be made to charge a battery from such…
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to YT2095 +1
    Thanks YT2095, I am thinking of developing a power supply that will work for a very long time if not forever when the components are capable of working forever, the system will involve 2x 12 volts batteries…
Parents
  • yaadsnap
    0 yaadsnap over 9 years ago

    Hello my name is Conroy and i am from Jamaica.. What if a inverter is being connected to a battery source to give out a AC energy of 120volts and you use back that 120AC energy to power a battery charger to charge back that same battery that needs to keep charge to keep the inverter going. Is that possible?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • yaadsnap
    0 yaadsnap over 9 years ago

    Hello my name is Conroy and i am from Jamaica.. What if a inverter is being connected to a battery source to give out a AC energy of 120volts and you use back that 120AC energy to power a battery charger to charge back that same battery that needs to keep charge to keep the inverter going. Is that possible?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • michaelkellett
    0 michaelkellett over 9 years ago in reply to yaadsnap

    It's perfectly possible, but quite useless.

     

    All the energy from the battery will be lost warming up the inverter and the battery. When you charge a battery you always need to put more energy in than you took out to get it back to the original state. ALL inverters are less than 100% efficient.

     

    There is no way to get energy for 'free' no matter how cleverly you connect up batteries or magnets.

     

     

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • rsc
    0 rsc over 9 years ago in reply to yaadsnap

    Think about this:

    To charge a 12V battery at 10A you need 120W.  If your inverter was 100% efficient, and all your wires had no resistance, you would need 120W back from the battery (10A).

    If your inverter is only 95% efficient, you would need 126W (10.5A).  So You are drawing 10.5A from the battery and only charging with 10A, your battery will soon be dead.

    It gets more complicated when you take battery resistance into account.  You can't just charge the battery at 12V, you need 14V or 15V to get current flowing into the battery.

    At 15V @ 10A, you are using 150W, so it would draw 12.5A from the battery charger at 12V, your battery is dying even faster.  Inside the inverter there are losses in the transformer, losses in the diodes and transistor junctions, and all the connecting wires have resistance, causing energy loss as heat.

    Scott