Power & Energy
  • Technologies
  • More
Power & Energy
Forum Is there any way a battery can charge other battery through isolated Charging circuit powered by a battery?
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 29 replies
  • Answers 6 answers
  • Subscribers 289 subscribers
  • Views 15347 views
  • Users 0 members are here
  • alternative_energy
  • energy_power
  • energy_storage
Related

Is there any way a battery can charge other battery through isolated Charging circuit powered by a battery?

e14 Contributor
e14 Contributor over 14 years ago

Hi all,

I am just thinking about developing a circuit to charged a 12 Volt battery and the charging circuit will be porwered by a second battery

  • Sign in to reply
  • Cancel

Top Replies

  • kkazem
    kkazem over 14 years ago +2 suggested
    Hi Uche, I'm a master power electronics engineer and I specialize in DC-DC converters, solar charge converters, DC-AC Inverters, Power Supplies, and battery chargers. Yes, you can charge a battery from…
  • YT2095
    YT2095 over 14 years ago +1 suggested
    a battery charger doesn`t care Where it gets its power from, be it mains, solar or another battery, as long as it`s capable of supplying enough power, a regulator can be made to charge a battery from such…
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to YT2095 +1
    Thanks YT2095, I am thinking of developing a power supply that will work for a very long time if not forever when the components are capable of working forever, the system will involve 2x 12 volts batteries…
Parents
  • YT2095
    0 YT2095 over 14 years ago

    a battery charger doesn`t care Where it gets its power from, be it mains, solar or another battery, as long as it`s capable of supplying enough power, a regulator can be made to charge a battery from such supply.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to YT2095

    Thanks YT2095,  I am thinking of developing a power supply that will work for a very long time if not forever when the components are capable of working forever, the system will involve 2x 12 volts batteries which could be of any amp, and 2x charger circuits, each of the charger circuit  will be simultaneously switching over in charging each other battery cells while both of them will power a load in a consecutive time, at this stage an MCU will be design with program to monitor ther charging period of one of the battery also enable the system to switch over the charger to the exhausted battery while the already charged battery will simutaneously take control of powering the same load.

    I would prefer that each of the power charging source to be on battery, only not solar because I presumed that the solar energy will sometime become weak mostly at night time, the intension of this project is due to an interrupted power supply in a developing counteries or in a remote rural villages that never have access to their own National Electric power supply . What do you think about   this?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • YT2095
    0 YT2095 over 14 years ago in reply to e14 Contributor

    I think I understand, it`s basically a UPS, with a spare back-up battery, so while one is in use, the other is charging, and when charged it will swap over with the other battery to charge that.

    I do something similar here in the Lab, only I took the internal battery leads outside of the UPS case, and swap the batteries manually when needed.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • YT2095
    0 YT2095 over 14 years ago in reply to e14 Contributor

    I think I understand, it`s basically a UPS, with a spare back-up battery, so while one is in use, the other is charging, and when charged it will swap over with the other battery to charge that.

    I do something similar here in the Lab, only I took the internal battery leads outside of the UPS case, and swap the batteries manually when needed.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to YT2095

    Yes it is similar function as the UPS, but the main technology invole is to electronically swap the battery lead to a charger circuit with the means of Microntroller to sence the limit in chargered current and simultaneously swap the charger circuit to the  empty battery, I also presumed that the both batteries will continually tied to the load in parallel connection, or will be a good ideal to interchange the Ouputs to a load?.

    Best Regards.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • YT2095
    0 YT2095 over 14 years ago in reply to e14 Contributor

    If I were to do that, i think I would leave the GNDs (the - terminals) common, and just switch in/out the Positive leads, probably with power relays as a Flip-Flop arrangement.

    your MCU would then only have to switch the base of a transistor to sink the current required for the relays at the right time (battery charged).

     

    edited to add: Thinking about it, you probably don`t even need an MCU at all! if the relays have a set dropout voltage, you can simply set it such that when a battery needs charging it cannot supply sufficient power to a relay, the field collapses and automatically switches in the new battery 5086.contentimage_1.png

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer