Power & Energy
  • Technologies
  • More
Power & Energy
Forum Is there any way a battery can charge other battery through isolated Charging circuit powered by a battery?
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 29 replies
  • Answers 6 answers
  • Subscribers 289 subscribers
  • Views 15324 views
  • Users 0 members are here
  • alternative_energy
  • energy_power
  • energy_storage
Related

Is there any way a battery can charge other battery through isolated Charging circuit powered by a battery?

e14 Contributor
e14 Contributor over 14 years ago

Hi all,

I am just thinking about developing a circuit to charged a 12 Volt battery and the charging circuit will be porwered by a second battery

  • Sign in to reply
  • Cancel

Top Replies

  • kkazem
    kkazem over 14 years ago +2 suggested
    Hi Uche, I'm a master power electronics engineer and I specialize in DC-DC converters, solar charge converters, DC-AC Inverters, Power Supplies, and battery chargers. Yes, you can charge a battery from…
  • YT2095
    YT2095 over 14 years ago +1 suggested
    a battery charger doesn`t care Where it gets its power from, be it mains, solar or another battery, as long as it`s capable of supplying enough power, a regulator can be made to charge a battery from such…
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to YT2095 +1
    Thanks YT2095, I am thinking of developing a power supply that will work for a very long time if not forever when the components are capable of working forever, the system will involve 2x 12 volts batteries…
Parents
  • kkazem
    0 kkazem over 14 years ago

    Hi Uche,

     

    I'm a master power electronics engineer and I specialize in DC-DC converters, solar charge converters, DC-AC Inverters, Power Supplies, and battery chargers. Yes, you can charge a battery from another battery, if that's what you're asking. I don't know why you need it isolated. However, I've got to agree with D2113F with reference to your other replies to this post. To me, it sounds like a perpetual motion machine wheras you have two batteries that are each connected to relays that can switch the individual batteries to either a load or to a a charging circuit fed by the other battery. Here is the problem. Battery-1 is connected to a load and is discharged to the point that you want to rechage it from the other battery that's been idle. Battery-2 recharges Battery-1 thru a dc-dc converter with a control to ensure that it's not overcharged. Now, Battery-2 is discharged and Battery-1 is charged, therefore, the relay or relays setup the circuit such that Battery-1 recharges Battery-2 and now Battery-1 is again discharged. Hopefully, you see where I'm going with this. It's an (almost) endless loop of the batteries charging and discharging each other. And if you powered a load first, discharging Battery-1, then recharged it with Battery-2, Battery-2 is now discharged and you can power the load only one more time with Battery-1. But now, you can no longer recharge Battery-1 with Battery-2 since Battery-2 is discharged, The only way around this is if you have some additional power from another Battery, or a Solar Cell, or from an AC-DC Power Supply to put the lost energy back into the system.

     

    One of the first things you should have learned in physics is that there is no such thing as a perpetual motion machine. Since you used the energy in Battery-1 to power the load and the energy in Battery-2 to recharge Battery-1, and since you used-up the energy in Battery-1 again powering the load after the recharge, you are out of energy as both Battery-1 and Battery-2 are discharged. Does this make any sense to you? I hope so, but if not, please feel free to reply here or send me a message using the Element-14 internal messaging system.

     

    Best regards,

    Kamran Kazem

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to kkazem

    Meet the Tesla 4-battery switch. Ever tried it? http://www.greenoptimistic.com/2008/01/29/how-to-build-a-tesla-4-battery-switch/

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • DAB
    0 DAB over 14 years ago in reply to e14 Contributor

    Hi Ovidiu,

     

    The article is very interesting.  I think what happens is that there is a slight time lag inside the battery from the time you begin loading the battery and to when it reaches a steady state.  By cycling the battery at higher frequency, you can get to the point where the electrical and chemical reactions reach a level of resonance, creating the short burst of extra electrons due to the chemical reaction collapse.

     

    If anyone has one of these working, I would love to know how long you can run the circuit until you get either a chemical depletion or some other failure.

     

    I really wish I understood electromagnetics as well as Tesla did.  The world truely lost a valuable resource when he died.

     

    Just my opinion,

    DAB

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to DAB

    Hi

     

    Thanks for your interesting contribution about the battery principle, I so much love your contribution to this article, I have been thinking in mind on developing a prototype simple battery and solar energy driven car, in this project I would like to perfect the energy source to be Kind of Forever energy supply, that is where I have this thought, My intention is to use two batteries one of the battery will start by powering an inverter of 12V to 230V AC, this inverter will as well power a dc 12v circuit that will be the motor control unite with PWM signal.

     

    The circuit will have a dc voltage output source to isolation circuit with Opto-isolate components, I am thinking that the batteries will be charging well when the charging current will be independent from the source, and this is the reason why I would love to apply that technique.

     

    I hope I am right with this ideal.

     

    Regards

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • DAB
    0 DAB over 14 years ago in reply to e14 Contributor

    I think to key to your idea will be both the current load and the battery drain and charge issues.

    The tesla approach did not indicate how long the circuit could sustain itself under load.  That is the key to having your idea work.  If the load exceeds the oscillating chemical/electrical recovery cycles, then you will probably be disappointed with the results.

    I must admit, it is an intriguing approach, so keep us updated on your results.

     

    Thanks and good luck,

    DAB

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • DAB
    0 DAB over 14 years ago in reply to e14 Contributor

    I think to key to your idea will be both the current load and the battery drain and charge issues.

    The tesla approach did not indicate how long the circuit could sustain itself under load.  That is the key to having your idea work.  If the load exceeds the oscillating chemical/electrical recovery cycles, then you will probably be disappointed with the results.

    I must admit, it is an intriguing approach, so keep us updated on your results.

     

    Thanks and good luck,

    DAB