Power & Energy
  • Technologies
  • More
Power & Energy
Forum Is there any way a battery can charge other battery through isolated Charging circuit powered by a battery?
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 29 replies
  • Answers 6 answers
  • Subscribers 289 subscribers
  • Views 15358 views
  • Users 0 members are here
  • alternative_energy
  • energy_power
  • energy_storage
Related

Is there any way a battery can charge other battery through isolated Charging circuit powered by a battery?

e14 Contributor
e14 Contributor over 14 years ago

Hi all,

I am just thinking about developing a circuit to charged a 12 Volt battery and the charging circuit will be porwered by a second battery

  • Sign in to reply
  • Cancel

Top Replies

  • kkazem
    kkazem over 14 years ago +2 suggested
    Hi Uche, I'm a master power electronics engineer and I specialize in DC-DC converters, solar charge converters, DC-AC Inverters, Power Supplies, and battery chargers. Yes, you can charge a battery from…
  • YT2095
    YT2095 over 14 years ago +1 suggested
    a battery charger doesn`t care Where it gets its power from, be it mains, solar or another battery, as long as it`s capable of supplying enough power, a regulator can be made to charge a battery from such…
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to YT2095 +1
    Thanks YT2095, I am thinking of developing a power supply that will work for a very long time if not forever when the components are capable of working forever, the system will involve 2x 12 volts batteries…
Parents
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    Hello all, this is my maiden post here, I've truely enjoyed learning from this community. 7485.contentimage_1.png

     

    This is a topic that continually seems to come up in the area of alternative energy a lot, for me anyway.  A while back I was evaluating a three coil Bedini SSG motor, it had four independent batteries.  Because the positive side of the source battery is connected to the negative of the charge battery(s) there is not a common.  To handle this I used DPDT latching relays to move the batteries between their role as source and charge, this seemed to work quite well and kept things isolated.

     

    Possibly this method of DPDT relays would work, latching to minimize power draw...?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    Hello all, this is my maiden post here, I've truely enjoyed learning from this community. 7485.contentimage_1.png

     

    This is a topic that continually seems to come up in the area of alternative energy a lot, for me anyway.  A while back I was evaluating a three coil Bedini SSG motor, it had four independent batteries.  Because the positive side of the source battery is connected to the negative of the charge battery(s) there is not a common.  To handle this I used DPDT latching relays to move the batteries between their role as source and charge, this seemed to work quite well and kept things isolated.

     

    Possibly this method of DPDT relays would work, latching to minimize power draw...?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • kkazem
    0 kkazem over 9 years ago in reply to e14 Contributor

    Actually, with the two batteries that you described with a common point (one pos, one neg), that is a common point and a single, higher voltage charger can charge both batteries at the same time since they are in series. The open circuit charge voltage needs to be higher than the two battery voltages added together in this case. There's no need to use complex relay switching.