Power & Energy
  • Technologies
  • More
Power & Energy
Forum Is there any way a battery can charge other battery through isolated Charging circuit powered by a battery?
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 29 replies
  • Answers 6 answers
  • Subscribers 289 subscribers
  • Views 15333 views
  • Users 0 members are here
  • alternative_energy
  • energy_power
  • energy_storage
Related

Is there any way a battery can charge other battery through isolated Charging circuit powered by a battery?

e14 Contributor
e14 Contributor over 14 years ago

Hi all,

I am just thinking about developing a circuit to charged a 12 Volt battery and the charging circuit will be porwered by a second battery

  • Sign in to reply
  • Cancel

Top Replies

  • kkazem
    kkazem over 14 years ago +2 suggested
    Hi Uche, I'm a master power electronics engineer and I specialize in DC-DC converters, solar charge converters, DC-AC Inverters, Power Supplies, and battery chargers. Yes, you can charge a battery from…
  • YT2095
    YT2095 over 14 years ago +1 suggested
    a battery charger doesn`t care Where it gets its power from, be it mains, solar or another battery, as long as it`s capable of supplying enough power, a regulator can be made to charge a battery from such…
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to YT2095 +1
    Thanks YT2095, I am thinking of developing a power supply that will work for a very long time if not forever when the components are capable of working forever, the system will involve 2x 12 volts batteries…
Parents
  • kkazem
    0 kkazem over 14 years ago

    Hi Uche,

     

    I'm a master power electronics engineer and I specialize in DC-DC converters, solar charge converters, DC-AC Inverters, Power Supplies, and battery chargers. Yes, you can charge a battery from another battery, if that's what you're asking. I don't know why you need it isolated. However, I've got to agree with D2113F with reference to your other replies to this post. To me, it sounds like a perpetual motion machine wheras you have two batteries that are each connected to relays that can switch the individual batteries to either a load or to a a charging circuit fed by the other battery. Here is the problem. Battery-1 is connected to a load and is discharged to the point that you want to rechage it from the other battery that's been idle. Battery-2 recharges Battery-1 thru a dc-dc converter with a control to ensure that it's not overcharged. Now, Battery-2 is discharged and Battery-1 is charged, therefore, the relay or relays setup the circuit such that Battery-1 recharges Battery-2 and now Battery-1 is again discharged. Hopefully, you see where I'm going with this. It's an (almost) endless loop of the batteries charging and discharging each other. And if you powered a load first, discharging Battery-1, then recharged it with Battery-2, Battery-2 is now discharged and you can power the load only one more time with Battery-1. But now, you can no longer recharge Battery-1 with Battery-2 since Battery-2 is discharged, The only way around this is if you have some additional power from another Battery, or a Solar Cell, or from an AC-DC Power Supply to put the lost energy back into the system.

     

    One of the first things you should have learned in physics is that there is no such thing as a perpetual motion machine. Since you used the energy in Battery-1 to power the load and the energy in Battery-2 to recharge Battery-1, and since you used-up the energy in Battery-1 again powering the load after the recharge, you are out of energy as both Battery-1 and Battery-2 are discharged. Does this make any sense to you? I hope so, but if not, please feel free to reply here or send me a message using the Element-14 internal messaging system.

     

    Best regards,

    Kamran Kazem

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to kkazem

    Mr. Kazem,

     

    I am no expert on this subject by far, but I do have a silly question.  Here is the example:  You have a 16,000mAh 6s Lipo Battery as a primary source of power.  This energy source provides power to a DC motor.  The DC motor turns and creates energy, which will provide a charge to the primary battery.

     

    Is this possible?  If it is, I would like to speak further with you on this.  Perhaps you can help develop something I have in mind.  Thanks!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to kkazem

    Mr. Kazem,

     

    I am no expert on this subject by far, but I do have a silly question.  Here is the example:  You have a 16,000mAh 6s Lipo Battery as a primary source of power.  This energy source provides power to a DC motor.  The DC motor turns and creates energy, which will provide a charge to the primary battery.

     

    Is this possible?  If it is, I would like to speak further with you on this.  Perhaps you can help develop something I have in mind.  Thanks!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • shabaz
    0 shabaz over 11 years ago in reply to e14 Contributor

    Double-post. Your question is also posted here:

    http://www.element14.com/community/thread/44536/l/battery-charging-using-dc-motor