Power & Energy
  • Technologies
  • More
Power & Energy
Forum Best switch mode design to step down 5-12v to 5v at 1A?
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 4 replies
  • Subscribers 285 subscribers
  • Views 1292 views
  • Users 0 members are here
  • buck
  • dc-dc
  • dc/dc
  • converter
  • power_conversion
Related

Best switch mode design to step down 5-12v to 5v at 1A?

e14 Contributor
e14 Contributor over 14 years ago

Hi,

I'm trying to design a switch mode step down buck regulator on my ATmega-based microcontroller board that will take 5-12+v from a LiPo or other power source and convert it to 5v with max current 1A.

I'm new to the field of power supplies/regulators, so I don't yet know exactly what would work well and what wouldn't.

 

I've looked at TI's TL2575 ICs, which are 1A "simple step-down switching regulators." Only four external components are needed (inductor, 2 caps, schottky diode), and it's 85+% efficient. The problem, however, is that it requires a big 330uH inductor that is expensive.

 

I then moved on to looking at another TI chip, the TPS63061 (kind of hard to find...just released in Dec. 2011). It is a buck-boost converter with 2A max current. This will allow for an input lower than 5v, as well as above it, so it would work great with 1/2-cell LiPo batteries. It uses a 1.5uH inductor, some small caps, a resistor, and a pretty big 66uF ceramic. Overall, the footprint is much smaller, but the total cost is a bit higher. Here's a basic schematic.

 

I've also been on WEBENCH and desiged a 6-18v input, 5v/1.6A output regulator with the TI LM20333.

 

What design would you suggest?

 

Thanks for the help!

Michael

  • Sign in to reply
  • Cancel
Parents
  • Catwell
    0 Catwell over 14 years ago

    Michael,

     

    Making a switching power supply like the TI LM20333 is an elegant solution.

     

    Could you get away with using a LM7805LM7805 or LM78XX series linear regulator? It would be the simplest, one component, option. The LM7805ACT.LM7805ACT. linked here can handle up to 20V input.

     

    Cabe

    http://twitter.com/Cabe_e14

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Catwell
    0 Catwell over 14 years ago

    Michael,

     

    Making a switching power supply like the TI LM20333 is an elegant solution.

     

    Could you get away with using a LM7805LM7805 or LM78XX series linear regulator? It would be the simplest, one component, option. The LM7805ACT.LM7805ACT. linked here can handle up to 20V input.

     

    Cabe

    http://twitter.com/Cabe_e14

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to Catwell

    I initially thought about using a simple linear regulator, but with the amount of current I would be using I'd probably have to put a heatsink on the board. I think it would be better to use a switch mode regulator to aim for most efficiency and low power dissipation (albeit a more complex design!)

    The LM20333 looks like a good solution, but I'm thinking maybe the TPS63061 would be even better because of its buck-boost SEPIC design and smaller inductor? I've never soldered SON/QFN packages before, but I just ordered a few Schmartboard breakout boards to help with the initial prototype.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • RWM
    0 RWM over 14 years ago in reply to e14 Contributor

    For input 12V and 1A load current heatsink would be big (7Watts) so it is better to use switching converter. I think you can try TPS63061 or check LM5000/5001 http://www.ti.com/product/lm5001