Power & Energy
  • Technologies
  • More
Power & Energy
Forum DC-DC Converter EOL replacement help
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 0 replies
  • Subscribers 282 subscribers
  • Views 616 views
  • Users 0 members are here
Related

DC-DC Converter EOL replacement help

failsafe
failsafe over 14 years ago

Hello Everybody,

 

I created a circuit that measures some analog sources and decodes some quad-encoders.  Its just about to go into production and would'nt you know it the 2" x 2" pcb mount DC-DC converter I was using is going EOL.  Now normally I wouldnt care too much and just replace it with another pcb mount DC-DC converter.  As it turns out, the DC-DC converter I originally picked has a feature that I need and cant find anywhere else.

 

 

The DC-DC converter I was using is this one PTK15-Q24-D5:  [url]http://parts.digikey.com/1/parts/731630-converter-dc-dc-5v-dual-out-ptk15-q24-d5.html[/url] and datasheet here http://products.cui.com/CUI_PTK15-Q24-D5_Datasheet.pdf?fileID=4499

 

 

The important feature that separates that DC-DC converter from most is:   It is a dual output (pos and neg) DC-DC converter with a trim port.  The trim port allows you to set the output to a non-standard value.  Trim ports are very common on single output DC-DC converters, but I haven't found another one on a Dual (pos/neg) DC-DC conv.

 

 

I used it on my circuit to take in 24VDC and output +/- 5.25V.  The total load of the circuit is just under 1A.  The 5.25V output (instead of a typical 5V) was needed in order for my Instrumentation Amps and ADC to span 0-5V.

Basically I need the overhead for the amps to hit 5V and to be able to use a LDO 5V reference for the ADC.

 

 

Just a couple considerations:

[list]

[li]Now, if I could find a drop-in replacement that would be great.  If I could find a 1" x 2" sized converter, even better.  I haven't found either.  [/li]

 

 

[li]Its gonna be low volume, so a custom part from another manufacturer is not possible.  Its gotta be an off the shelf part.[/li]

[li]I saw some other much higher wattage DC-DC converters with a trim port, but I cant use them.  My circuit wont supply the necessary minimum load to ensure voltage regulation.[/li]

[li]I cant add resistors to increase my current usage in order to be able to use the higher wattage converters because the 24Vdc supply feeds multiple circuits.[/li]

[/list]

 

 

I am gonna keep looking and if anyone has any parts suggestion, I am all ears.

I figured I'd checkout Newark and Element14 for a replacement part.  Maybe I just need to look at a different selection of manufacturers.

 

 

If I can't find a drop-in replacement my initial inclination is to replace the DC-DC with a linear regulator to create the required +5.25V.  Then I would use a small DC-DC converter (buck, inverting) to create -1V.

Note:  The negative rail is just so the instrumentation amplifiers can hit 0V.

I would like to hear people's advice on how they would deal with this situation.

 

 

 

 

Thanks guys,

-Karl