Power & Energy
  • Technologies
  • More
Power & Energy
Forum Any one using LM2577(voltage regulator)
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 7 replies
  • Subscribers 284 subscribers
  • Views 1402 views
  • Users 0 members are here
  • dc-dc
  • current
  • converter
  • power
  • energy
Related

Any one using LM2577(voltage regulator)

e14 Contributor
e14 Contributor over 14 years ago

Hi,

 

 

I am trying to use a voltage step up circuit. And I have brought a LM2577T(voltage regulator) for stepping up the out voltage.

After I connecting the circuit properly as the technical datasheet from element14 shows.

The output voltage with no load is around 12(input voltage is 5 voltage).

But unluckily the output voltage drops to 3 voltage directly when I connect a load of 200 ohms.

Could you tell me why the load will drop the output voltage and how to avoid the issue?

 

 

Thanks very much!

Michael

Attachments:
image
  • Sign in to reply
  • Cancel
  • mberman
    0 mberman over 14 years ago

    Hi Michael,

    Suggest you make sure the input current "Is" meets this device's specs.

    If it does, suggest you contact Texas Instruments to resolve this issue.

    Best regards,

    Mel

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Nortski
    0 Nortski over 14 years ago

    Hello Michael,

    You might want to check the value of the capacitor across the input of the regulator.  TI says 0.1uF, but other diagrams like the test circuit say a 220uF capacitor should be used.  The ripple current may be causing problems with the 5V input circuit.  As Mel says, contact TI to check.

    Thanks

    David

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • RWM
    0 RWM over 14 years ago

    I had similar problem with control circuit TPS40210.

    What is nominal current of choke coil 100uH? Have you used 0.1uF on input and 680uF on output?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to RWM

    Hi,

     

    I have connected the exact same circuit as I have seen from the data sheet.

     

    I have not measured the Inom, however as I am using a DC power source in lab, I think it shouldn't be a problem for the source to supply enough current.

     

     

    What could be the other factor ?

     

    Thank you very much for your kind reply =)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to Nortski

    Hi,

     

    May I know what what do you mean by ripple current may be causing a problem?

     

    I have tried several capacitor value and the same thing happen - voltage drops as soon as I connect it to a load like dc fan / dc motor/ LED.

     

    Thank you very much for your kind reply. =)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • RWM
    0 RWM over 14 years ago in reply to e14 Contributor

    Hi,

     

    not ripple current but maximum allowed coil current can cause problem. Do you have specifications of choke coil?

     

    Sometimes also big internal resistance of capacitors can cause problems. Do you have specifications of capacitors or information on manufacturer/type?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago

    Hi,

    I use this circuit in 2 projects. I had a problems with transitions between high load and low or no load. I had also problems with circuit startup with AC adapter and laboratory power source. Behavior of this circuit was always different. Sometimes DC/DC was very "noisy" or in some undefined state. Solution was in compensation network. I changed capacitor in comp. network and everything was ok. In my situation was value of capacitor quite far from calculated values. From my previous experiences with switching power converters I often use paralel combination of ESR electrolyth capacitor and small ceramic or 1uF tantalum capacitor on inputs and outputs.