Power & Energy
  • Technologies
  • More
Power & Energy
Forum Beginner's Project: ATX Benchtop Power Supply
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 7 replies
  • Answers 2 answers
  • Subscribers 285 subscribers
  • Views 1006 views
  • Users 0 members are here
Related

Beginner's Project: ATX Benchtop Power Supply

e14 Contributor
e14 Contributor over 14 years ago

Hi,

 

As one of my first real projects, I would like to build an benchtop power supply based on an ATX power supply. I'm not planning to modify the power supply itself, but I would like to add a circuit to it to allow a couple of things. I'm a programmer so maybe my instinct of going right away for a microcontroller is bad, but since I would like it to have only one output with a voltage selector (I was thinking of adding an LCD screen and using a clickable rotary switch to make it good looking) to cycle between the ATX's -12V, 3.3V, 5V, 12V and maybe add a voltage regulator for other voltages, it seemed easier to control transistors on each rails to control which one is active or not.

 

While this flow makes sense in my head (4 lines - -12V, 3.3V, 5V and 12V - merging into a single one with transistors acting as "gates" and I guess diodes for safety?), it somehow doesn't sound safe... is it?  I haven't seen a similar build on the internet... people tend to expose each rail invidually... but I think it would be a better learning experience for me to make it work with a single output rail.

 

Any feedback is greatly appreciated before I fry anything image

 

Thanks!

  • Sign in to reply
  • Cancel

Top Replies

  • e14 Contributor
    e14 Contributor over 14 years ago +2
    So, I spent a few hours learning Eagle and reading some open source schematics as "tutorial" / inspiration... I want to build an enclosure for this thing, so most things are linked to terminal posts as…
  • YT2095
    YT2095 over 14 years ago +1 suggested
    these psu`s can output several 10`s of amps, transistors aren`t a good idea for this without significant wastage. personally I would go with Relays and use the rotary switch to activate those, also you…
Parents
  • YT2095
    0 YT2095 over 14 years ago

    these psu`s can output several 10`s of amps, transistors aren`t a good idea for this without significant wastage. personally I would go with Relays and use the rotary switch to activate those, also you`ll need a break before make type.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • YT2095
    0 YT2095 over 14 years ago

    these psu`s can output several 10`s of amps, transistors aren`t a good idea for this without significant wastage. personally I would go with Relays and use the rotary switch to activate those, also you`ll need a break before make type.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to YT2095

    The relays sound like the best/safest approach.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer