Power & Energy
  • Technologies
  • More
Power & Energy
Forum Ideas to obtain 12VDc from 400VAc
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 283 subscribers
  • Views 682 views
  • Users 0 members are here
Related

Ideas to obtain 12VDc from 400VAc

e14 Contributor
e14 Contributor over 13 years ago

Hi everyone!

I want to desing a power supply to obtain an output of 12V from an input in the range of 85V-400V AC or DC.It has to supply 3W. I've thought to use electronic transformers, (myrra 47134) that some of its advantages are high performance, wide range of input voltages and operating indistinct both AC and DC. They accept an input of 85-265VAC y 85-370VDC, so I think a topology like this to achieve 400V input.

For low voltages, the input sections of the two transformers are connected in parallel. A relay is activated when the input voltage exceeds 200V so that both transformers will be connected in series.

 

image

These transformers are based on flayback topology so I begin to think that when they work in series the gorund of the high transformer will be floating so it will turn crazy and I begin to think that it won't be able to work

Someone has some idea to transfor this input? are there any comercial product which can help me?

Thanks

Attachments:
imageMyrra 47134.pdf
  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    Hi

    try to use a normal powerint device http://www.powerint.com then put some power zener  zener on HV line (between rectifier diode and input capacitor) like voltage drop device.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    Hi

    try to use a normal powerint device http://www.powerint.com then put some power zener  zener on HV line (between rectifier diode and input capacitor) like voltage drop device.