Power & Energy
  • Technologies
  • More
Power & Energy
Forum Maximising power output from solar panels
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 14 replies
  • Answers 1 answer
  • Subscribers 289 subscribers
  • Views 3314 views
  • Users 0 members are here
  • micro-inverter
  • solar_tracker
  • micro_inverters
  • mppt
  • solar
  • tracking_systems
Related

Maximising power output from solar panels

e14 Contributor
e14 Contributor over 13 years ago

There is an ongoing debate in the sector about how best to maximise the power from a solar panel and minimise shading effects: do you use a micro-inverter with built in MPPT or do you use a solar tracker. Both have cost implications, but what is your preference from a technical viewpoint?

  • Sign in to reply
  • Cancel

Top Replies

  • Catwell
    Catwell over 13 years ago +1
    Although I am not in the alternative energy industry, I would have to lean towards the MPPT option. For stationary panels, the MPPT option is best for choosing the best location for maximum output. However…
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to bad_boy_y +1
    Sounds good to me, but the amount of copper would be more to use 12v since you lose more power in the line for a given power transmission. Think about it, to send 100watts through the line you would need…
Parents
  • smartengineer
    0 smartengineer over 13 years ago

    Hi, James.

    I think that the loss of productivity is associated with the occurrence of the thermal noise due to heating solar panels.
    The solution - is to cool solar panels to a temperature , eliminating the appearance of thermal noise in a semiconductor crystal, if possible.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • smartengineer
    0 smartengineer over 13 years ago

    Hi, James.

    I think that the loss of productivity is associated with the occurrence of the thermal noise due to heating solar panels.
    The solution - is to cool solar panels to a temperature , eliminating the appearance of thermal noise in a semiconductor crystal, if possible.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to smartengineer

    Thermal noise is a problem in signal circuitry but in power circuitry it is smoothed by capacitance in the regulator circuitry, however thermal noise can be a problem when the silicon gets to a temperature where thermal runaway takes place, shorting the plates. Fortunately silicon has a very high critical temperature.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • sbkenn
    0 sbkenn over 12 years ago in reply to smartengineer

    Cooled to what ?  Kelvin is the relevant scale.  Cooling by 10C is going to use more energy than you gain from the PV.

    On another point, that of MPPT, I suggest that, in order to charge batteries to the maximum, the PV would need to charge a large capacitor, then through a buck-boost converter, so that even in low light conditions, some power would be acquired.  The converter would determine where the MPP is, and draw current from the PV/capacitor into the the batteries to meet MPP requirements.

    Plain ol' PWM won't do that, regardless of it's intelligence.  This is particularly relevant where average light isn't great.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • nihaomike
    0 nihaomike over 12 years ago in reply to sbkenn

    A big capacitor is not necessary. In low light, just slow down the charging. That does mean that many off the shelf charger chips are not suitable for this use.