Power & Energy
  • Technologies
  • More
Power & Energy
Forum Maximising power output from solar panels
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 14 replies
  • Answers 1 answer
  • Subscribers 289 subscribers
  • Views 3306 views
  • Users 0 members are here
  • micro-inverter
  • solar_tracker
  • micro_inverters
  • mppt
  • solar
  • tracking_systems
Related

Maximising power output from solar panels

e14 Contributor
e14 Contributor over 13 years ago

There is an ongoing debate in the sector about how best to maximise the power from a solar panel and minimise shading effects: do you use a micro-inverter with built in MPPT or do you use a solar tracker. Both have cost implications, but what is your preference from a technical viewpoint?

  • Sign in to reply
  • Cancel

Top Replies

  • Catwell
    Catwell over 13 years ago +1
    Although I am not in the alternative energy industry, I would have to lean towards the MPPT option. For stationary panels, the MPPT option is best for choosing the best location for maximum output. However…
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to bad_boy_y +1
    Sounds good to me, but the amount of copper would be more to use 12v since you lose more power in the line for a given power transmission. Think about it, to send 100watts through the line you would need…
Parents
  • bad_boy_y
    0 bad_boy_y over 13 years ago

    One big lost  is the use of inverter but lot of thing run on 12v or under. After the wall wart lost power again and they use power when is not in use. Lot of home electronic use 12v but have internal power supply to use 120v ac. maybe we need 12v line in the new(green) home.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to bad_boy_y

    With many inverters having efficiences better than 95% I don't think you can say this is a big loss.  If you don't want to upgrade wiring sizes to use the lower voltage (12V or 24/48VDC) then an inverter is the only way to go, sure you get double conversions taking place but in most cases the loss is small enough to not be an issue.  Systems size obviously needs to take any losses into account but generous oversizing always seems to be the best policy anyway.  I run my house as such and don't find that there is anything I am concerned about and the system will have more than paid for itself after 5 years of use.  At 5 years plus I am expecting to see ageing effects with the batteries and they will eventually require replacement but that is a minimal expense given the overall benefits.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to bad_boy_y

    With many inverters having efficiences better than 95% I don't think you can say this is a big loss.  If you don't want to upgrade wiring sizes to use the lower voltage (12V or 24/48VDC) then an inverter is the only way to go, sure you get double conversions taking place but in most cases the loss is small enough to not be an issue.  Systems size obviously needs to take any losses into account but generous oversizing always seems to be the best policy anyway.  I run my house as such and don't find that there is anything I am concerned about and the system will have more than paid for itself after 5 years of use.  At 5 years plus I am expecting to see ageing effects with the batteries and they will eventually require replacement but that is a minimal expense given the overall benefits.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer