Power & Energy
  • Technologies
  • More
Power & Energy
Forum Maximising power output from solar panels
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 14 replies
  • Answers 1 answer
  • Subscribers 289 subscribers
  • Views 3312 views
  • Users 0 members are here
  • micro-inverter
  • solar_tracker
  • micro_inverters
  • mppt
  • solar
  • tracking_systems
Related

Maximising power output from solar panels

e14 Contributor
e14 Contributor over 13 years ago

There is an ongoing debate in the sector about how best to maximise the power from a solar panel and minimise shading effects: do you use a micro-inverter with built in MPPT or do you use a solar tracker. Both have cost implications, but what is your preference from a technical viewpoint?

  • Sign in to reply
  • Cancel

Top Replies

  • Catwell
    Catwell over 13 years ago +1
    Although I am not in the alternative energy industry, I would have to lean towards the MPPT option. For stationary panels, the MPPT option is best for choosing the best location for maximum output. However…
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to bad_boy_y +1
    Sounds good to me, but the amount of copper would be more to use 12v since you lose more power in the line for a given power transmission. Think about it, to send 100watts through the line you would need…
Parents
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    Regardless of the mechanism for concentration of solar input, dust and other barrier particulate materials will degrade you power output over the long term - particularly when you rely on a protective covering for the PV panels that can be affected by the environment (pitting, oxidation, etc) that decreases your output. For traditional PV panels, cooling the substrate will allow for thermo-voltaic conversion while simultaneously improving the PV panel's output for the same input radiance. I used this process with submerged flexible panels in the Solar Seaweed design, which was intended to also use piezoelectric film to capture wave energy as well.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    Regardless of the mechanism for concentration of solar input, dust and other barrier particulate materials will degrade you power output over the long term - particularly when you rely on a protective covering for the PV panels that can be affected by the environment (pitting, oxidation, etc) that decreases your output. For traditional PV panels, cooling the substrate will allow for thermo-voltaic conversion while simultaneously improving the PV panel's output for the same input radiance. I used this process with submerged flexible panels in the Solar Seaweed design, which was intended to also use piezoelectric film to capture wave energy as well.