Power & Energy
  • Technologies
  • More
Power & Energy
Forum Best, most efficient way to get 5WDC from 120VAC 60Hz
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 4 replies
  • Subscribers 284 subscribers
  • Views 804 views
  • Users 0 members are here
  • current
  • ac-dc
  • power_management
  • converter
  • Design
  • power_supply
  • power_conversion
  • power
  • energy
  • regulator
Related

Best, most efficient way to get 5WDC from 120VAC 60Hz

nathanjseeley
nathanjseeley over 13 years ago

First off, Not sure if this is the right place to be posting this, but I need help.

 

So I am working on making some phone chargers (my friend is knitting the "enclosures" for them, they are really cute) I am looking for the best way to take Standard US Household voltage and drop it to +5VDC.

 

I have two thoughts and am wondering which would be the best.

 

1. Use a chain of voltage regulators and a rectifying bridge to drop the voltage (more heat, possibly less weight)

 

2. Use a transformer to drop it from 120VAC to 12VAC then put it through the bridge and a 5V regulator (less heat, possibly heavier)

 

Which of these methods would you guys suggest, also is there going to be more to the circuit than just the Transformers, regulators and their associated hardware?

  • Sign in to reply
  • Cancel

Top Replies

  • e14 Contributor
    e14 Contributor over 13 years ago +1
    Best, most efficient way would be to build a switch mode power supply by rectifying your ac directly to +/- 170 volts dc, then using a control unit turn it back to Ac at about 100 KHz or higher. This would…
Parents
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    Best, most efficient way would be to build a switch mode power supply by rectifying your ac directly to +/- 170 volts dc, then using a control unit turn it back to Ac at about 100 KHz or higher. This would enable you to use it on alot smaller transformer that in part gives you a greater efficiency, about 98%. So after you have 170 volt at 100 KHz you can with the help of your transformer turn into the required voltage. After that just recitify it again and you will have your Dc.

     

    The switch mode power supply can be build alot smaller and cheaper because of the transformer being use at higher frequency is ALOT smaller and cheaper than these needed for the standerd 60 Hz.

    You could always put a regulator on the output just to be sure but that limit the amount of current that can be use before the regulator over-heats.

     

    These switch modes are mostly use for high current and smaller sizes, like the chagers you get with most devices are all switch modes.

    The control unit I was talking about is usually a "PWM" pulse width modulation unit that turn the dc into a square wave for the transformar to be able to induce magnetic currents.

    Hope this helps.image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    Best, most efficient way would be to build a switch mode power supply by rectifying your ac directly to +/- 170 volts dc, then using a control unit turn it back to Ac at about 100 KHz or higher. This would enable you to use it on alot smaller transformer that in part gives you a greater efficiency, about 98%. So after you have 170 volt at 100 KHz you can with the help of your transformer turn into the required voltage. After that just recitify it again and you will have your Dc.

     

    The switch mode power supply can be build alot smaller and cheaper because of the transformer being use at higher frequency is ALOT smaller and cheaper than these needed for the standerd 60 Hz.

    You could always put a regulator on the output just to be sure but that limit the amount of current that can be use before the regulator over-heats.

     

    These switch modes are mostly use for high current and smaller sizes, like the chagers you get with most devices are all switch modes.

    The control unit I was talking about is usually a "PWM" pulse width modulation unit that turn the dc into a square wave for the transformar to be able to induce magnetic currents.

    Hope this helps.image