Power & Energy
  • Technologies
  • More
Power & Energy
Forum MOSFET recomendation for LTC4008 Li-ion Charger (5 cells pack)
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 16 replies
  • Answers 4 answers
  • Subscribers 282 subscribers
  • Views 3029 views
  • Users 0 members are here
  • mosfet
  • battery
  • charger
Related

MOSFET recomendation for LTC4008 Li-ion Charger (5 cells pack)

e14 Contributor
e14 Contributor over 13 years ago

Hi,

 

I´m currently designing a 5 cell pack Li-ion charger with LTC4008 chip (discussion posted in Sep 2011 in this thread)

In page 15 of LTC4008 datasheet you can find the topic about the MOSFET selection.

 

I´m certainly lost in the proper selection. I know that logic-level MOSFETS must be used (gate voltage around (5.6V-6V), but is the first time for me designing with mosfets.

 

One important point is the output voltage of the carger, datasheet says that if Vout>20V then the RDSon should be little more high for reducing the ripple...

 

The charge voltage will be 20.5V and maximum Output Current 1.5A

 

I was thinking on use the mosfets that appear in the schematics of the datasheet, but has anyone any recommendation?, I mean, do I have to go deep in the mosfets area or can I use one recommended by anyone who has be involved in similar scenarios?

 

The only important thing in this design is the proper selection for minimum ripple current, at cost of something (as always). Efficiency for example is not a problem cause it´s a battery charger (I prefer to lost energy efficency if that means reduce ripple current in the output). I´m thinking to use a slightly high Inductor (around 40 microH) and two low ESR tantalum capacitors "surge robust" in parallel in the output of the mosfets.

 

Any comments are appreciated

 

PS: I need reference values. (What means high ... what means low... 0.001 - 0.01 ? (in mosfet parameters)

  • Sign in to reply
  • Cancel

Top Replies

  • Pradipsinh
    Pradipsinh 6 months ago in reply to Pradipsinh +1 suggested
    7.2 ah battery charger use Ltc4008 which mosfet runnig
Parents
  • shabaz
    0 shabaz over 13 years ago

    I'd go with the ones used in their eval board here. 20.5V is borderline higher than 20V so determining the effect of RDSon without any further details may need to be experimental.

    The MOSFETs in their eval board look appropriate for your charge voltage, assuming the input is less than 25V or so (to not operate against max thresholds). The gate voltage of both the MOSFETs is low,

    and the datasheet specifies the p-channel gate voltage range (VCLP-VTGATE) to be well below -20V for the on condition (and below 50mV when off, so the MOSFETs will certainly switch off) and you're safe there too.

    I havn't confirmed power dissipation you should expect, but that should be an easy calculation, based on the RDSon value, and is likely fine.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to shabaz

    The same mosfets appear in LTC4008 datasheet (page 20)...

     

    Q1: Si4431BDY

    Q2: FDC645N

     

    These MOSFETS has RDSon quite low, they are recommended for less than 20Vin

    My DCin is 24V and the maximum voltage applied to the Battery will be 20.5V (avoiding 90-100% duty cycle width pulse)

    I think those mosfets will work (rated to 30V I guess), but for sure there are another mosfets more adequate for this scenario...

     

    We talk about Vin<20V... and I have 24V

     

    extract from page 16 datasheet:

     

    "For VIN < 20V the high current efficiency generally improves with larger MOSFETs, while for VIN > 20V the transition losses rapidly increase to the point that the use of a higher RDS(ON) device with lower CRSS actually provides higher efficiency. The synchronous MOSFET losses are greatest at high input voltage or during a shortcircuit when the duty cycle in this switch in nearly 100%"

     

    image

     

    Thanks for the patience

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 13 years ago in reply to e14 Contributor

    Ah, sorry, I'd gone with your original post "datasheet says that if Vout>20V then the RDSon should be little more high" and assumed it matched the datasheet.

    They've got the formulas in the datasheet to calculate the power dissipation, just plug in the CRSS and RDS(ON) values from the MOSFET datasheets (CRSS is in

    a graph) (and they've got an approximation for the temperature dependency too) and an estimate for the constant k that they use in the formulas is there too.

     

    I ran the formula for the P-ch, and got a value of the order of 50mW, using values of 20.5V, 25V, 0.04ohms, 1.5A, 100pF and 300kHz

    for the parameters involved. I could be wrong, so worth double-checking.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to shabaz

    True, I say Vout where it should be Vin>20V

     

    Anyway, thanks for the help but that demo board is for 4 cells max, and the design differences between charging 4 and 5 cells is greater than the expected. That´s why I´m using LTC4008 (instead of LTC4007 li-ion dedicated)... even the mosfets used should change, and I dont find any reference for a recommendation using 5 cell battery charger. can you believe it? well, it is. And why that demoboard limit the charge to 4 cells? when LTC4008 can charge even until 6 cells!. Something happen when crossing the gap... charging more than 4 cells is odd... I´m just taking precautions in this journey my friend

     

    Regards

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to shabaz

    True, I say Vout where it should be Vin>20V

     

    Anyway, thanks for the help but that demo board is for 4 cells max, and the design differences between charging 4 and 5 cells is greater than the expected. That´s why I´m using LTC4008 (instead of LTC4007 li-ion dedicated)... even the mosfets used should change, and I dont find any reference for a recommendation using 5 cell battery charger. can you believe it? well, it is. And why that demoboard limit the charge to 4 cells? when LTC4008 can charge even until 6 cells!. Something happen when crossing the gap... charging more than 4 cells is odd... I´m just taking precautions in this journey my friend

     

    Regards

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • shabaz
    0 shabaz over 13 years ago in reply to e14 Contributor

    True, very good to take precautions for these types of circuits! I really don't like designing chargers

    to be honest (I've seen what happens when things go wrong to batteries).

    I too wondered, but the eval pdf mentions the limit is due to the capacitor ratings on the board.

    I think it's worth prototyping up with the same MOSFETs, and sticking a scope on the MOSFETs

    to confirm no limit is being exceeded on any spikes, and that the power dissipation is as expected.

    The paper exercise seems to indicate it should work with the same MOSFETs.

    Also, any such circuit should be tested at different temperatures. Good luck, and be careful -

    batteries are exceedingly dangerous. Worth monitoring parameters (current, temperature) of them

    while doing any tests.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to shabaz

    EDITED:

     

    Totally agree.

     

    I had also a very crazy experience but with an assasing CC/CC that killed every mosfet plugged to it during months...(finally was a bug in that family of chips) in this case is even worst because the explosives. I will look for Polimer Lithium Batteries (stronger and less explosives) and also test it inside an iron box or something similar...

     

    I like the idea of later change the mosfets if I discover better ones, but designing first with these "non-fitted" transistors

    The battery pack I will use will have of course all the protections inside (if not, that would be really dangerous indeed!). The only protection not included is the thermistor network that is easy to implement with the LTC4008. So I hope it would not explode! image

     

    Thanks a lot for the tips.

     

    Cheers.

     

    PS: I leave the topic open, maybe someone appear and has developed a 5 cell battery charger...