Power & Energy
  • Technologies
  • More
Power & Energy
Forum wind power & pv system
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 1 reply
  • Subscribers 283 subscribers
  • Views 405 views
  • Users 0 members are here
  • wind
  • Alternative Energy Tags
  • power
  • pv_module
Related

wind power & pv system

e14 Contributor
e14 Contributor over 13 years ago

How to add wind power & pv system as a input to a buck converter?

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    A buck converter refers to a method of changing the voltage of a supply by regulating the output of a smoothed transformer secondary winding. You are "bucking" or kicking the voltage up or down. Another name is switching regulator or DC to DC supply or inverte/dropper. A solar PV panel generates power in the form of DC voltage and current. If it is fed into a buck converter it will produce a voltage regulated output within the power rating of the solar array and the buck converter. So if the panel produces 200watts at 25volts the input current will be 4amps and the output current will depend on the voltage regulated and its load - V^2/R=I^2*R=W. If the sun doesn't shine the power output will drop and the buck converter should maintain the voltage as long as V(in)>V(out)+V(drop). Similar sort of reasoning would apply to wind generation, though the supply would be from an alternator driven by the propeller, and hence AC.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    A buck converter refers to a method of changing the voltage of a supply by regulating the output of a smoothed transformer secondary winding. You are "bucking" or kicking the voltage up or down. Another name is switching regulator or DC to DC supply or inverte/dropper. A solar PV panel generates power in the form of DC voltage and current. If it is fed into a buck converter it will produce a voltage regulated output within the power rating of the solar array and the buck converter. So if the panel produces 200watts at 25volts the input current will be 4amps and the output current will depend on the voltage regulated and its load - V^2/R=I^2*R=W. If the sun doesn't shine the power output will drop and the buck converter should maintain the voltage as long as V(in)>V(out)+V(drop). Similar sort of reasoning would apply to wind generation, though the supply would be from an alternator driven by the propeller, and hence AC.