Power & Energy
  • Technologies
  • More
Power & Energy
Forum LM317 in parallel - Answered -> LM2596 circuit question
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 20 replies
  • Answers 2 answers
  • Subscribers 289 subscribers
  • Views 8624 views
  • Users 0 members are here
Related

LM317 in parallel - Answered -> LM2596 circuit question

ckambiselis
ckambiselis over 13 years ago

Hello,

 

I am building a DC-DC converter to convert the 14.8v 6A power coming from a professional camera battery to 9V 2.5A used by a DSLR, I am trying to build this converter using the LM317 since it's the only easily available power regulator (which I don't have to order 2500pcs to place an order), the problem is the LM317 can only output 1.5A max, can I build the circuit using 2 of them and connecting the outputs of each circuit in paralel to get 9V 3A, is there going to be any kind of problem that may fry the camera?

 

Thank you

Oscar

 

Message was edited by: Christos Oscar Kambiselis

  • Sign in to reply
  • Cancel

Top Replies

  • mconners
    mconners over 13 years ago in reply to johnbeetem +2
    In the LM 317 datasheet http://www.ti.com/lit/ds/symlink/lm317.pdf (sorry about the pdf) figure 13 on page 12 shows three of them in parallel (of course with supporting circuitry) to create an adjustable…
  • e14 Contributor
    e14 Contributor over 13 years ago +2 suggested
    I invented the Lm317. It is NOT designed to be paralleled. If you parallel devices, one will supply all the current until it thermally or current limits and then the other one will come on. This not reliable…
  • mconners
    mconners over 13 years ago +1
    One thing to keep in mind is that you said you will be running this off of a battery. I think John Beetem is correct in asserting that you will be generating quite a bit of heat with this circuit. Heat…
Parents
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    I invented the Lm317.   It is NOT designed to be paralleled. If you parallel devices, one will supply all the current until it thermally or current limits and then the other one will come on.  This not reliable.

     

    The data sheet show circuitry that allow paralleling by forcing current sharing. A new device, the LT3081 is designed for easy sharing. Also the LT 3080

     

     

    Bob Dobkin

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • vtrandal
    0 vtrandal over 5 years ago in reply to e14 Contributor

    Bob [Bob Dobkin], your reply in this forum seems largely unnoticed. Thank you for inventing the LM317 and creating such a useful device [and revenue engine] that I am just now learning about. And thank you for suggesting the newer LT3081 and LT3080 as alternatives when needing more current than one LM317 can provide.

     

    Regarding voltage sources in general I think putting battery cells in parallel also has problems. The cells will eventually drain each other unless something is done to prevent that.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • vtrandal
    0 vtrandal over 5 years ago in reply to e14 Contributor

    Bob [Bob Dobkin], your reply in this forum seems largely unnoticed. Thank you for inventing the LM317 and creating such a useful device [and revenue engine] that I am just now learning about. And thank you for suggesting the newer LT3081 and LT3080 as alternatives when needing more current than one LM317 can provide.

     

    Regarding voltage sources in general I think putting battery cells in parallel also has problems. The cells will eventually drain each other unless something is done to prevent that.