Power & Energy
  • Technologies
  • More
Power & Energy
Forum LM317 in parallel - Answered -> LM2596 circuit question
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 20 replies
  • Answers 2 answers
  • Subscribers 288 subscribers
  • Views 8673 views
  • Users 0 members are here
Related

LM317 in parallel - Answered -> LM2596 circuit question

ckambiselis
ckambiselis over 13 years ago

Hello,

 

I am building a DC-DC converter to convert the 14.8v 6A power coming from a professional camera battery to 9V 2.5A used by a DSLR, I am trying to build this converter using the LM317 since it's the only easily available power regulator (which I don't have to order 2500pcs to place an order), the problem is the LM317 can only output 1.5A max, can I build the circuit using 2 of them and connecting the outputs of each circuit in paralel to get 9V 3A, is there going to be any kind of problem that may fry the camera?

 

Thank you

Oscar

 

Message was edited by: Christos Oscar Kambiselis

  • Sign in to reply
  • Cancel

Top Replies

  • mconners
    mconners over 13 years ago in reply to johnbeetem +2
    In the LM 317 datasheet http://www.ti.com/lit/ds/symlink/lm317.pdf (sorry about the pdf) figure 13 on page 12 shows three of them in parallel (of course with supporting circuitry) to create an adjustable…
  • e14 Contributor
    e14 Contributor over 13 years ago +2 suggested
    I invented the Lm317. It is NOT designed to be paralleled. If you parallel devices, one will supply all the current until it thermally or current limits and then the other one will come on. This not reliable…
  • mconners
    mconners over 13 years ago +1
    One thing to keep in mind is that you said you will be running this off of a battery. I think John Beetem is correct in asserting that you will be generating quite a bit of heat with this circuit. Heat…
Parents
  • ckambiselis
    0 ckambiselis over 13 years ago

    I actually found an assembled LM2596 circuit in a really small package from a Chinese eBay seller for only 1.05 pounds with free postage, with 1 year warranty, ordered 5 of them :-P

     

    Well since I found a better solution for my problem, only one question remains, what would be the ideal placement of a heatsink to this board (since if using it with a greater than 15W load it is recomended) would I have to only cool the chip or the whole unit, by the way this will be placed inside a solid aluminum small box measuring about 8x5x5cm , would it be better to mill the block so that it fits exactly inside, so the case itself is a heatsink, or do you believe it would get too hot.

     

    Module photo:

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • ckambiselis
    0 ckambiselis over 13 years ago

    I actually found an assembled LM2596 circuit in a really small package from a Chinese eBay seller for only 1.05 pounds with free postage, with 1 year warranty, ordered 5 of them :-P

     

    Well since I found a better solution for my problem, only one question remains, what would be the ideal placement of a heatsink to this board (since if using it with a greater than 15W load it is recomended) would I have to only cool the chip or the whole unit, by the way this will be placed inside a solid aluminum small box measuring about 8x5x5cm , would it be better to mill the block so that it fits exactly inside, so the case itself is a heatsink, or do you believe it would get too hot.

     

    Module photo:

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • sqkybeaver
    0 sqkybeaver over 13 years ago in reply to ckambiselis

    it looks like the regulator is heatsunk through the ground plane. the switching regulators are much more efficent than a linear regulator. a moderate air flow around the board should do the trick.