Power & Energy
  • Technologies
  • More
Power & Energy
Forum Charging 3V coin cell battery
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 2 replies
  • Subscribers 283 subscribers
  • Views 2455 views
  • Users 0 members are here
Related

Charging 3V coin cell battery

e14 Contributor
e14 Contributor over 12 years ago

Hi everyone,

 

I am currently trying to design a very small power source for an embedded project. My current idea is to use a rechargable coin cell battery (e.g. Panasonic ML-1220).

A boost converter (e.g. tps61025) would provide system power. The load will be connected only for a few seconds per hour and draw about 2mA when connected. A capacitor will be used to mitigate spike current draw.

Maybe I would add something like bq27501 as a battery charge gauge.

 

My current problem is to design a charging circuit for this project. It must take power from USB, and recharge a 3V Manganese Lithium coin cell battery. All of the battery

charging controllers that I found aim at 4.2V charging voltage or higher, while a coin cell specification (http://industrial.panasonic.com/www-data/pdf/AAA4000/AAA4000PE17.pdf) requires 3.1V charging voltage.

Could someone advise some solution to recharge these batteries? If I use a voltage divider on the charging output of, say, bq24018 it would just draw current from the battery when idle and would completely undermine the performace.

Are there any smarter solutions to this problem?

 

Thanks for your help!

Vlad.

  • Sign in to reply
  • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    So far I found this document: http://www.intersil.com/content/dam/Intersil/documents/tb45/tb456.pdf

    Is it going to be safe enough to trickle charge those batteries?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • michaelkellett
    0 michaelkellett over 12 years ago in reply to e14 Contributor

    Hello Vlad,

     

    follow the link to Panasonic's recommended charging circuit - and note the warning:

     

    Under no circumstances should trickle charging, which is used for nickel-cadmium batteries, be used. Ignoring

    this precaution will cause the battery voltage to rise to about 5V, resulting in a deterioration of performance.

     

    http://industrial.panasonic.com/www-data/pdf/AAA4000/AAA4000PE17.pdf

     

    You just need a voltage regulator and a resistor - no need for bqxxxx image

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer