Power & Energy
  • Technologies
  • More
Power & Energy
Forum Beginner question: 12V wall wart to power both a msp430 microcontroller and an LED strip
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 4 replies
  • Answers 2 answers
  • Subscribers 284 subscribers
  • Views 894 views
  • Users 0 members are here
Related

Beginner question: 12V wall wart to power both a msp430 microcontroller and an LED strip

e14 Contributor
e14 Contributor over 12 years ago

Hi all

 

I wish to make a circuit, where I control an LED strip  from a msp430 microcontroller (a MSP430G2231 that came with the MSP430 Launchpad). It needs 1.8-3.6V. The LED strip needs 12V. And yes, this IS for gaudy christmas lights :-)

 

I think I have figured out to control the LED strip through a MOSFET.

 

So the question is all about the power supply.

I figure that the easiest option would be to run the LED strip of a separate 3V coin cell battery as the msp430 doesn't use much power.

 

But if I wanted to avoid batteries, what would easiest and cheapest way to convert the 12V from a salvaged small wall wart to ~3V?

This is what I have been looking into:

 

  • 7805 (5V) ICs seem to be readily available, but I have not seen a 7803. Could you drop the final 2v, maybe by using a diode of some sort?
  • Other option is equally available LM317 and hardwired adjustment resistors.

 

These are linear options, right? I guess that during to the low current draw of the msp430, heat is not a huge worry?

 

Am I way off?

  • Sign in to reply
  • Cancel

Top Replies

  • e14 Contributor
    e14 Contributor over 12 years ago in reply to jvdberg@ieee.org +1
    Thank you for a helpful answer. As far as my novice reading of the datasheet, the lm138 is able to carry more current than a lm317, but similar in function, right? My local electronics guy has the lm317…
Parents
  • jvdberg@ieee.org
    0 jvdberg@ieee.org over 12 years ago

    You can use the LM138 regulator. This regulator has 3 pins, like the 7805, but the voltage can be set using two resistors. The minimum Voltage is 1.25 Volt.

    This regulator is also available in TO3 version, that can handle more power.

    See the datasheet at

    http://pdf.datasheetcatalog.com/datasheet/nationalsemiconductor/DS009060.PDF

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to jvdberg@ieee.org

    Thank you for a helpful answer.

     

    As far as my novice reading of the datasheet, the lm138 is able to carry more current than a lm317, but similar in function, right? My local electronics guy has the lm317 on stock, and since my microcontroller uses power in the micro-amp range, I think the lm317 is right for my use.

     

    Datasheet: http://pdf.datasheetcatalog.com/datasheet/nationalsemiconductor/DS009063.PDF

     

    Or am I missing something?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to jvdberg@ieee.org

    Thank you for a helpful answer.

     

    As far as my novice reading of the datasheet, the lm138 is able to carry more current than a lm317, but similar in function, right? My local electronics guy has the lm317 on stock, and since my microcontroller uses power in the micro-amp range, I think the lm317 is right for my use.

     

    Datasheet: http://pdf.datasheetcatalog.com/datasheet/nationalsemiconductor/DS009063.PDF

     

    Or am I missing something?